cancel
Showing results for 
Search instead for 
Did you mean: 

cannot load flash programming algorithm error

Ss.61
Associate III

*I am using stm32f7508-DK ,

*Under ==>

[ STM32Cube\Repository\STM32Cube_FW_F7_V1.16.0\Projects\

STM32F7508-DISCO->Demonstrations->STemWin ]

*It gives error img attached ,

* Expect help to resolve this part.

3 REPLIES 3

Probably better asking Keil-specific questions on the Keil forum:

https://community.arm.com/support-forums/f/keil-forum

The 'Build Output' window seems to be giving you the reason why it failed to load Flash Algorithms:

0693W00000NsNK9QAN.png

Amel NASRI
ST Employee

Hi @Ss.6​ ,

Try to follow steps as described in "How to use it ? " section at the readme.txt file of the example.

Is same problem still faced?

-Amel

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Go into settings for Debugger are and increase the RAM size allocated, perhaps to 0xE000 from 0x1000 or whatever

0693W00000Nsoy1QAB.jpg

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..