2020-10-31 1:56 AM
After my lost battle with H750 and H745, I wanted to have a small win. However, it doesn't work like that. I took my F769 disco board and flashed the most basic sample project in touchgfx - directly from touchgfx, no modification on the interface/code. The display went black and did not want to work even I reset/unplugged the board.
Tried with the sample demo for F769 from ST site- black display also -- both tried to flash from ST utility and CubeProgrammer( I have 2.6.alpha cube programmer).
I then tried the Embedded wizard demo for F769 and to my surprise, running their flashing master demo works.
I have TouchGFX 4.15.0 & Cube Programmer 2.6 alpha.
What am i doing wrong?
2020-11-01 10:50 PM
Hello,
Please provide the steps.
I have tried with my F769 disco and everything works perfectly.
The only thing different that I see different so far is that I use CubeProgrammer 2.5 but I don't think that would be the issue.
Maybe could you give the version of your board ? Mine is MB1225B. And the display is MB1166 Rev A.
/Alexandre