2024-11-07 04:40 AM
I am looking for a breakthrough to integrate TouchGFX with the STM32U575I-EV. However, the GIT repo for STM32U5 does not have any of such example.
I tried using the STMCubeMX with the base IOC file for the eval board and integrated TouchGFX with it. However, after building the firwmare successfully, the image does not show up on the display at start.
Any example can I have to refer and understand what I am missing? It is really hard for a developer to start using TOuchGFX and STM environment even while using the eval board and speed up the prototyping activities.
2024-11-08 07:43 AM
Hi @mdalal ,
This post has been escalated to the ST Online Support Team for additional assistance. We'll contact you directly.
Kind Regards
2024-11-08 07:53 AM
Same question in here already escalated.