cancel
Showing results for 
Search instead for 
Did you mean: 

Any example of TouchGFX and STM32U575I-EV integration

mdalal
Associate III

I am looking for a breakthrough to integrate TouchGFX with the STM32U575I-EV. However, the GIT repo for STM32U5 does not have any of such example.

I tried using the STMCubeMX with the base IOC file for the eval board and integrated TouchGFX with it. However, after building the firwmare successfully, the image does not show up on the display at start.

Any example can I have to refer and understand what I am missing? It is really hard for a developer to start using TOuchGFX and STM environment even while using the eval board and speed up the prototyping activities. 

2 REPLIES 2
Osman SOYKURT
ST Employee

Hi @mdalal ,

This post has been escalated to the ST Online Support Team for additional assistance. We'll contact you directly. 

Kind Regards

Osman SOYKURT
ST Software Developer | TouchGFX
SofLit
ST Employee

Same question in here already escalated.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.