2021-07-25 08:30 AM
Hello,
I worked with TouchGFX 4.16.1 fine, because of graph issue in 4.16, i've migrated to TouchGFX 4.17 and also CubeMX 6.3 ... after this updating touchgfx_init() function produce hardfault .... Please help me how can I solve this issue ....
I work with STM32H743 ... D-cache enable ... dual buffer , External SDRAM...
Solved! Go to Solution.
2021-10-03 01:48 AM
Check two extra things.
1- do you initiate your external flash before touchgfx init?
2- Make some delay with Hal_Delay function about 500 ms before peripherals initializing, It helps if some device need more time after resetting to be functional.
I hope it will help..
2021-07-25 09:27 AM
Hello,
I also create a new project with touchGFX4.17 from scratch without any success ....
2021-07-25 09:29 AM
When reached to this line ... hard fault accured ....
Bitmap::registerBitmapDatabase(BitmapDatabase::getInstance(), BitmapDatabase::getInstanceSize());
Please help
2021-08-30 01:25 AM
digging this up and linking this post to the other post your created on the same issue
2021-09-23 01:29 AM
Hello, i had the same problem with my disco board (f746g) yesterday. I don't know why, but in the debugger settings there was no external loader set anymore. After set it it worked fine.
2021-09-23 03:22 AM
Hi,
Was it the same scenario where you migrated a project from TouchGFX 4.16.1 to 4.17 ? What version of STM32CubeMX are you using ? Did you start a proejct from scratch or from the TBS for the STM32F746G-DISCO board available in TouchGFX Designer ?
Could you confirm that disabling the external flash loader causes your project to hard fault ? That seems strange .
/Romain
2021-09-30 11:22 AM
Hi MDani,
All of my problem after updating is solved when I decided to migrate from KEIL to STM32CubeIDE, It seems Keil has some bugs in this case
I suggest if you are using keil, probably your problem will solve after migrating to STM ide....
BR,
2021-10-02 11:53 PM
Yes Romain, i migrated a the project from 4.16.1 to 4.17 and i also updated the STM32CubeIDE from 1.6.0 to 1.7, after that the problem occured. It was a new project i created.
Ok, now I'm very confused, I really thought the problem came from disabling the external loader. Now i tried it again with the external flash disabled but I didn't get a hard fault. But I'm really sure that was the only thing i changed to get it to work.
Anyway, it works.
Hey Haji, no I do not use the Keil IDE, I'm already working with the CubeIDE, but thank you for the hint.
2021-10-03 01:48 AM
Check two extra things.
1- do you initiate your external flash before touchgfx init?
2- Make some delay with Hal_Delay function about 500 ms before peripherals initializing, It helps if some device need more time after resetting to be functional.
I hope it will help..