2020-08-05 9:35 AM
Hi Martin,
I just updated my huge project from release 4.12.0 to 4.13.0 (skipped 4.13.) and generated the sources after a few minor changes.
Now Keil can not find the source files for the images anymore, because TouchGFX now placed an "image_" ahead in the file names.
I have 360 images !!! I would have to eliminate all images from the project and add the new ones in place. This is actually a time consuming job! Is there a way to get the files created as the prevois version ???
Note: I can't use the project file which is created by TouchGFX, because I have created my job long ago with one of the first versions and without CubeMX support and had to set up my project manually - you might remember this.
Thanks for any suggestions. Gaby.
Solved! Go to Solution.
2020-08-28 3:12 AM
Hi Gaby,
We did the "image_" prefix because prefixing variables with "_" does not respect the c++ specification. (Imaging if you had an asset called main.cpp). It would generate a symbol"_main" which is protected.
/Martin
2020-08-05 10:34 AM
Ok, finally I've done the project file names conversion... Project working again.
2020-08-28 3:12 AM
Hi Gaby,
We did the "image_" prefix because prefixing variables with "_" does not respect the c++ specification. (Imaging if you had an asset called main.cpp). It would generate a symbol"_main" which is protected.
/Martin
2020-08-28 7:00 AM
Ok, thanks for the info, Martin!