‎2021-11-14 09:12 PM
I created an simulator project, but I can’t run it.
The log is as follows:
Generate Code
Copy Framework
Copying TouchGFX framework version 4.18.0 to E:\ljc\Projects\STM32Projects\touchgfx_test\Middlewares\ST\touchgfx
Done
Generate
Wrote config/gcc/app.mk
Wrote config/msvs/Application.props
Wrote generated/gui_generated/include/gui_generated/common/FrontendApplicationBase.hpp
Wrote generated/gui_generated/include/gui_generated/common/FrontendHeapBase.hpp
Wrote generated/gui_generated/include/gui_generated/common/SimConstants.hpp
Wrote generated/gui_generated/include/gui_generated/screen_screen/screenViewBase.hpp
Wrote generated/gui_generated/src/common/FrontendApplicationBase.cpp
Wrote generated/gui_generated/src/screen_screen/screenViewBase.cpp
Wrote generated/simulator/gcc/Makefile
Wrote generated/simulator/include/simulator/mainBase.hpp
Wrote generated/simulator/include/simulator/video/DirectFrameBufferVideoController.hpp
Wrote generated/simulator/include/simulator/video/MJPEGDecoder.hpp
Wrote generated/simulator/include/simulator/video/SoftwareMJPEGDecoder.hpp
Wrote generated/simulator/msvs/touchgfx_prebuild.targets
Wrote generated/simulator/msvs/touchgfx_sdl2.props
Wrote generated/simulator/msvs/touchgfx.props
Wrote generated/simulator/src/mainBase.cpp
Wrote generated/simulator/src/video/SoftwareMJPEGDecoder.cpp
Wrote generated/simulator/touchgfx.ico
Wrote generated/simulator/touchgfx.rc
Wrote generated/simulator/touchgfx.res
Wrote gui/include/gui/common/FrontendApplication.hpp
Wrote gui/include/gui/common/FrontendHeap.hpp
Wrote gui/include/gui/model/Model.hpp
Wrote gui/include/gui/model/ModelListener.hpp
Wrote gui/include/gui/screen_screen/screenPresenter.hpp
Wrote gui/include/gui/screen_screen/screenView.hpp
Wrote gui/src/common/FrontendApplication.cpp
Wrote gui/src/model/Model.cpp
Wrote gui/src/screen_screen/screenPresenter.cpp
Wrote gui/src/screen_screen/screenView.cpp
Wrote simulator/gcc/Makefile
Wrote simulator/main.cpp
Wrote simulator/msvs/Application.sln
Wrote simulator/msvs/Application.vcxproj
Wrote simulator/msvs/Application.vcxproj.filters
Done
Generate Assets
make -f simulator/gcc/Makefile assets -j8
'MySQL' �?是内部或外部命令,也�?是�?��?行的程�?
或批处�?�文件。
'MySQL' �?是内部或外部命令,也�?是�?��?行的程�?
或批处�?�文件。
Failed
Failed
I tried demos and examples and got the same error.
'MySQL' is not an internal or external command, nor is it an executable program or batch file.
I don't know how to solve it, can anyone help me?:loudly_crying_face:
‎2021-11-14 09:21 PM
An exception occurred when I opened the demo.
2021-11-15 13:14:50,041 [1] INFO TouchGFXDesigner.App: Logging configured
2021-11-15 13:15:16,179 [1] INFO TouchGFXDesigner.Main.MainWindow: Application started
2021-11-15 13:15:16,180 [1] INFO TouchGFXDesigner.Main.MainWindow: Username: luoji
2021-11-15 13:15:16,180 [1] INFO TouchGFXDesigner.Main.MainWindow: Designer version: 4.18.0
2021-11-15 13:15:16,180 [1] INFO TouchGFXDesigner.Main.MainWindow: Designer installation path: C:\TouchGFX\4.18.0\designer
2021-11-15 13:15:16,180 [1] INFO TouchGFXDesigner.Main.MainWindow: Windows version: Microsoft Windows NT 10.0.19043.0
2021-11-15 13:15:16,181 [1] INFO TouchGFXDesigner.Main.MainWindow: Current culture: zh-CN
2021-11-15 13:15:16,185 [1] INFO TouchGFXDesigner.Main.MainWindow: Current culture time seperator: :
2021-11-15 13:15:16,185 [1] INFO TouchGFXDesigner.Main.MainWindow: Current culture date seperator: /
2021-11-15 13:15:16,192 [1] INFO TouchGFXDesigner.Main.MainWindow: Installed .NET version(s): v2.0.50727 2.0.50727.4927 SP2v3.0 3.0.30729.4926 SP2v3.5 3.5.30729.4926 SP1v4 (Client 4.8.04084 Full 4.8.04084 ) v4.0 (Client 4.0.0.0 )
2021-11-15 13:15:16,336 [11] INFO Utils.WebHandling.WebHandler: Downloading STM32F429I_DK_BUTTON_SAMPLE_DEMO.png
2021-11-15 13:15:16,976 [11] ERROR Utils.WebHandling.WebHandler: Response status code does not indicate success: 404 (Not Found).
System.Net.Http.HttpRequestException: Response status code does not indicate success: 404 (Not Found).
at System.Net.Http.HttpResponseMessage.EnsureSuccessStatusCode()
at Utils.WebHandling.FileDownloadUtil.DownloadFile(Uri uri, String filePath, IProgress`1 progress, Action completion, Action`1 bytesReceived)
at Utils.WebHandling.WebHandler.DownloadFile(Uri uri, String filePath, IProgress`1 progress, Action completion, Action`1 bytesReceived)
2021-11-15 13:15:16,991 [11] ERROR TouchGFXPackages.Implementation.FileDownloader: Failed to download: http://sw-center.st.com/touchgfx/pacman/4.18.0/STM32F429_DK_BUTTON_SAMPLE_DEMO/STM32F429I_DK_BUTTON_SAMPLE_DEMO.png
2021-11-15 13:15:30,526 [11] INFO Utils.WebHandling.WebHandler: Downloading STM32F429I_DK_BUTTON_SAMPLE_DEMO.png
2021-11-15 13:15:31,017 [11] ERROR Utils.WebHandling.WebHandler: Response status code does not indicate success: 404 (Not Found).
System.Net.Http.HttpRequestException: Response status code does not indicate success: 404 (Not Found).
at System.Net.Http.HttpResponseMessage.EnsureSuccessStatusCode()
at Utils.WebHandling.FileDownloadUtil.DownloadFile(Uri uri, String filePath, IProgress`1 progress, Action completion, Action`1 bytesReceived)
at Utils.WebHandling.WebHandler.DownloadFile(Uri uri, String filePath, IProgress`1 progress, Action completion, Action`1 bytesReceived)
2021-11-15 13:15:31,017 [11] ERROR TouchGFXPackages.Implementation.FileDownloader: Failed to download: http://sw-center.st.com/touchgfx/pacman/4.18.0/STM32F429_DK_BUTTON_SAMPLE_DEMO/STM32F429I_DK_BUTTON_SAMPLE_DEMO.png
2021-11-15 13:15:48,256 [19] INFO Utils.WebHandling.WebHandler: Downloading STM32F469I-DISCO-3.0.5.tpa
2021-11-15 13:15:50,453 [19] DEBUG TouchGFXPackages.Implementation.TouchGFXPackageStream: Filestream opened on C:\Users\luoji\AppData\Roaming\TouchGFX-4.18.0\Downloads\STM32F469I-DISCO\3.0.5\STM32F469I-DISCO-3.0.5.tpa
2021-11-15 13:15:50,466 [19] DEBUG TouchGFXPackages.Implementation.TouchGFXPackageStream: Filestream opened on C:\Users\luoji\AppData\Roaming\TouchGFX-4.18.0\Downloads\DiceAnimation\1.1.0\DiceAnimation-1.1.0.tpa
2021-11-15 13:15:50,502 [19] DEBUG TouchGFXPackages.Implementation.TouchGFXPackageStream: Filestream opened on C:\Users\luoji\AppData\Roaming\TouchGFX-4.18.0\Downloads\STM32F469I-DISCO\3.0.5\STM32F469I-DISCO-3.0.5.tpa
2021-11-15 13:15:50,859 [19] DEBUG TouchGFXPackages.Implementation.TouchGFXPackageStream: Filestream opened on C:\Users\luoji\AppData\Roaming\TouchGFX-4.18.0\Downloads\DiceAnimation\1.1.0\DiceAnimation-1.1.0.tpa
2021-11-15 13:15:51,281 [19] DEBUG TouchGFXDomainModel.Texts.TextManager: Loaded 477 fonts
2021-11-15 13:15:51,442 [19] ERROR TouchGFXDomainModel.LoadSave.LoadSave: 'MySQL' �?是内部或外部命令,也�?是�?��?行的程�?
或批处�?�文件。
'MySQL' �?是内部或外部命令,也�?是�?��?行的程�?
或批处�?�文件。
System.Exception: 'MySQL' �?是内部或外部命令,也�?是�?��?行的程�?
或批处�?�文件。
'MySQL' �?是内部或外部命令,也�?是�?��?行的程�?
或批处�?�文件。
at TouchGFXDomainModel.LoadSave.Update.Update4170To4180.ConvertExcelToXml(String pathToTextConverter, String pathToExcelFile, String pathToXmlFile)
at TouchGFXDomainModel.LoadSave.Update.Update4170To4180.Run()
at TouchGFXDomainModel.LoadSave.Update.UpdateSerial.Update4170To4180(String serial4170, String projectPath)
at TouchGFXDomainModel.LoadSave.Update.UpdateSerial.Update(String jsonString, String projectPath)
at TouchGFXDomainModel.LoadSave.Update.UpdateSerial.Run(String path)
at TouchGFXDomainModel.LoadSave.LoadSave.LoadDotTouchgfx(String filename)
at TouchGFXDomainModel.LoadSave.LoadSave.Load(String filename)
2021-11-15 13:15:51,448 [1] ERROR TouchGFXDesigner.App: Object reference not set to an instance of an object.
System.NullReferenceException: Object reference not set to an instance of an object.
at TouchGFXPackages.ImportExport.ImportGui.Import()
at TouchGFXPackages.Implementation.PackageManager.CombineAtAndUi(TouchGFXPackage tgui, TouchGFXPackage tgat, String projectPath, String applicationName, Int32 height, Int32 width, ColorDepth selectedColorDepth, IProgress`1 progressPercentage)
at TouchGFXDesigner.Main.Lobby.ApplicationCreatorOperation.<>c__DisplayClass5_0.<CombinePackagesAsync>b__0()
at System.Threading.Tasks.Task`1.InnerInvoke()
at System.Threading.Tasks.Task.<>c.<.cctor>b__277_0(Object obj)
at System.Threading.ExecutionContext.RunFromThreadPoolDispatchLoop(Thread threadPoolThread, ExecutionContext executionContext, ContextCallback callback, Object state)
--- End of stack trace from previous location ---
at System.Threading.Tasks.Task.ExecuteWithThreadLocal(Task& currentTaskSlot, Thread threadPoolThread)
--- End of stack trace from previous location ---
at TouchGFXDesigner.Main.Lobby.ApplicationCreatorOperation.CombinePackagesAsync(ApplicationCombineConfig applicationConfig, IProgress`1 progressPercentage)
at TouchGFXDesigner.Main.Lobby.ApplicationCreatorOperation.Create(ApplicationCombineConfig applicationConfig, IProgress`1 progressPercentage)
at TouchGFXDesigner.Main.Lobby.ApplicationCreator.ApplicationCreatorViewModel.CreateApplication(Object obj)
at System.Threading.Tasks.Task.<>c.<ThrowAsync>b__140_0(Object state)
at System.Windows.Threading.ExceptionWrapper.InternalRealCall(Delegate callback, Object args, Int32 numArgs)
at System.Windows.Threading.ExceptionWrapper.TryCatchWhen(Object source, Delegate callback, Object args, Int32 numArgs, Delegate catchHandler)
2021-11-15 13:18:51,728 [1] ERROR TouchGFXDesigner.App: Object reference not set to an instance of an object.
System.NullReferenceException: Object reference not set to an instance of an object.
at TouchGFXPackages.ImportExport.ImportGui.Import()
at TouchGFXPackages.Implementation.PackageManager.CombineAtAndUi(TouchGFXPackage tgui, TouchGFXPackage tgat, String projectPath, String applicationName, Int32 height, Int32 width, ColorDepth selectedColorDepth, IProgress`1 progressPercentage)
at TouchGFXDesigner.Main.Lobby.ApplicationCreatorOperation.<>c__DisplayClass5_0.<CombinePackagesAsync>b__0()
at System.Threading.Tasks.Task`1.InnerInvoke()
at System.Threading.Tasks.Task.<>c.<.cctor>b__277_0(Object obj)
at System.Threading.ExecutionContext.RunFromThreadPoolDispatchLoop(Thread threadPoolThread, ExecutionContext executionContext, ContextCallback callback, Object state)
--- End of stack trace from previous location ---
at System.Threading.Tasks.Task.ExecuteWithThreadLocal(Task& currentTaskSlot, Thread threadPoolThread)
--- End of stack trace from previous location ---
at TouchGFXDesigner.Main.Lobby.ApplicationCreatorOperation.CombinePackagesAsync(ApplicationCombineConfig applicationConfig, IProgress`1 progressPercentage)
at TouchGFXDesigner.Main.Lobby.ApplicationCreatorOperation.Create(ApplicationCombineConfig applicationConfig, IProgress`1 progressPercentage)
at TouchGFXDesigner.Main.Lobby.ApplicationCreator.ApplicationCreatorViewModel.CreateApplication(Object obj)
at System.Threading.Tasks.Task.<>c.<ThrowAsync>b__140_0(Object state)
at System.Windows.Threading.ExceptionWrapper.InternalRealCall(Delegate callback, Object args, Int32 numArgs)
at System.Windows.Threading.ExceptionWrapper.TryCatchWhen(Object source, Delegate callback, Object args, Int32 numArgs, Delegate catchHandler)
‎2021-11-14 09:41 PM
I solved this problem myself.
The reason is that mysql is installed on my computer, and everything is normal after uninstalling.
😂