2021-06-22 9:00 PM
2021-06-22 10:49 PM
Hello Jzhan.8,
Could you tell us in English the steps you did to arrive to this unexpected error ? Can you reproduce it ?
/Alexandre
2021-06-22 10:55 PM
OK,After using stm32cubemx to generate GUI code, I open the application template.touchgfx.part file in the project directory TouchGFX, and the designer reports an error. Error: I can't perform runtime binding on null reference. How can I solve this problem?Thanks~
2021-06-22 10:58 PM
Yes,I can reproduce it,it always does that,I haven't sloved it yet.
2021-06-22 11:05 PM
When I used STM32CUBEMX to generate GUI code,it's not appearing any warning and wrong.
2021-06-22 11:10 PM
Hi Jzhan.8,
Could you enclose your .touchgfx.part (and .touchgfx files if you have it) ?
/Alexandre
2021-06-22 11:19 PM
Can I add your Wechat or QQ?I can send it to you through it.
2021-06-23 12:03 AM
Unfortunately I don't have WeChat nor QQ.
You can send it to me by private message on this community.
/Alexandre
2021-06-23 12:33 AM
I haved sent it to you through privacy communication.
2021-06-23 1:19 AM
Your touchgfx.part is empty. It should not happen.
Can you tell me exactly the steps you did to generate it ?
Did you use CubeMX, add the TouchGFX Generator additional software to your project and generate code ?
/Alexandre