STM32G4 CRC8 with user polynomial doesn't match other method
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-09-07 3:46 PM
Hello, there,
I need CRC8 in my design. Thinking with the Polynomial programmability in Stm32G4 . It should be straight forward.
When I tried to test with the example "CRC_UserDefinedPolynomial" coming with stm32cube_fw_g4_v130 in "Examples_LL" folder, the result (0xA6) matches the "expected value" set in the code.
However, when the same group of the data is tested with other CRC calculator for Poly 0x9B, eg. https://crccalc.com/, the result is 0x88 instead of 0xA6.
Then I tried another example (different data set 0x1, 0x2, 0x3, 0x4) with HAL, the result doesn't match either.
The CRC hardware is a blackbox so I couldn't figure it out why. Is there anyone having running into similar issue and knowing the cause of the mismatch?
I would like to appreciate any inputs.
Thanks.
Solved! Go to Solution.
- Labels:
-
CRC
-
STM32G4 series
Accepted Solutions
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-09-08 11:21 AM
Thanks to the OPs who viewed this thread, especially @waclawek.jan and @TDK. Just to update in case it can be helpful to anyone may run into it.
I dug a little more in the Calculate_CRC() of the example, seems the original code trying to use the 32B capacity as much as possible even for CRC8, should be more efficiently if possible, but it's over my head and didn't work for me.
With a minor mods to just use 8B data feed, now the result matches the other calculator.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-09-07 3:59 PM
Post input, polynomial, initial value, expected output, real output.
JW
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-09-07 4:11 PM
Also keep in mind the polynomial is just one part of the CRC. The Initial value, RefIn, RefOut and XorOut will also affect the result.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-09-07 4:35 PM
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-09-07 4:36 PM
Hi, JW,
Thank you for your attention.
Here is the settings( all copied from the example since I just want to test :(
the files are in \STM32Cube\Respository\STM32Cube_FW_G4_V1.3.0\Projects\NUCLEO-G474RE\Examples_LL\CRC\CRC_UserDefinedPolynomial
void MX_CRC_Init(void)
{
/* Peripheral clock enable */
LL_AHB1_GRP1_EnableClock(LL_AHB1_GRP1_PERIPH_CRC);
LL_CRC_SetInputDataReverseMode(CRC, LL_CRC_INDATA_REVERSE_NONE);
LL_CRC_SetOutputDataReverseMode(CRC, LL_CRC_OUTDATA_REVERSE_NONE);
LL_CRC_SetPolynomialCoef(CRC, LL_CRC_DEFAULT_CRC32_POLY);
LL_CRC_SetPolynomialSize(CRC, LL_CRC_POLYLENGTH_32B);
LL_CRC_SetInitialData(CRC, LL_CRC_DEFAULT_CRC_INITVALUE);
/* USER CODE BEGIN CRC_Init 2 */
/* Configure CRC calculation unit with user defined polynomial value, 8-bit long */
LL_CRC_SetPolynomialCoef(CRC, CRC8_POLYNOMIAL_VALUE);
LL_CRC_SetPolynomialSize(CRC, LL_CRC_POLYLENGTH_8B);
/* USER CODE END CRC_Init 2 */
}
#define BUFFER_SIZE 39
#define CRC8_POLYNOMIAL_VALUE 0x9B
/* USER CODE BEGIN PV */
__IO uint8_t ubCRCValue = 0;
static const uint8_t aDataBuffer[BUFFER_SIZE] =
{
0x21, 0x10, 0x00, 0x00, 0x63, 0x30, 0x42, 0x20, 0xa5, 0x50, 0x84, 0x40,
0xe7, 0x70, 0xc6, 0x60, 0x4a, 0xa1, 0x29, 0x91, 0x8c, 0xc1, 0x6b, 0xb1,
0xce, 0xe1, 0xad, 0xd1, 0x31, 0x12, 0xef, 0xf1, 0x52, 0x22, 0x73, 0x32,
0xa1, 0xb2, 0xc3
};
/* Expected CRC Value */
uint8_t ubExpectedCRCValue = 0xA6;
........
main()
{
LL_APB2_GRP1_EnableClock(LL_APB2_GRP1_PERIPH_SYSCFG);
LL_APB1_GRP1_EnableClock(LL_APB1_GRP1_PERIPH_PWR);
NVIC_SetPriorityGrouping(NVIC_PRIORITYGROUP_4);
/* System interrupt init*/
/** Disable the internal Pull-Up in Dead Battery pins of UCPD peripheral
*/
LL_PWR_DisableUCPDDeadBattery();
/* USER CODE END PV */
SystemClock_Config();
/* USER CODE BEGIN SysInit */
/* USER CODE END SysInit */
/* Initialize all configured peripherals */
MX_GPIO_Init();
MX_CRC_Init();
/* USER CODE BEGIN 2 */
/* Perform CRC calculation on data contained in aDataBuffer */
ubCRCValue = Calculate_CRC(BUFFER_SIZE);
/* Check if CRC computed result value is equal to expected one */
CheckCRCResultValue();
/* USER CODE END 2 */
/* Infinite loop */
/* USER CODE BEGIN WHILE */
while (1)
{
/* USER CODE END WHILE */
/* USER CODE BEGIN 3 */
}
/* USER CODE END 3 */
}
uint8_t Calculate_CRC(uint32_t BufferSize)
{
register uint32_t data = 0;
register uint32_t index = 0;
/* Compute the CRC of Data Buffer array*/
for (index = 0; index < (BufferSize / 4); index++)
{
data = (uint32_t)((aDataBuffer[4 * index + 3] << 24) | (aDataBuffer[4 * index + 2] << 16) | (aDataBuffer[4 * index + 1] << 8) | aDataBuffer[4 * index]);
LL_CRC_FeedData32(CRC, data);
}
/* Last bytes specific handling */
if ((BUFFER_SIZE % 4) != 0)
{
if (BUFFER_SIZE % 4 == 1)
{
LL_CRC_FeedData8(CRC, aDataBuffer[4 * index]);
}
if (BUFFER_SIZE % 4 == 2)
{
LL_CRC_FeedData16(CRC, (uint16_t)((aDataBuffer[4 * index + 1] << 8) | aDataBuffer[4 * index]));
}
if (BUFFER_SIZE % 4 == 3)
{
LL_CRC_FeedData16(CRC, (uint16_t)((aDataBuffer[4 * index + 1] << 8) | aDataBuffer[4 * index]));
LL_CRC_FeedData8(CRC, aDataBuffer[4 * index + 2]);
}
}
/* Return computed CRC value */
return (LL_CRC_ReadData8(CRC));
}
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-09-07 4:39 PM
Hi, TDK,
I understand possible impact of the parameters you mentioned. But to my understanding, even those match, the result still doesn't match.
Thanks.
YW
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-09-07 4:48 PM
Observe content of CRC registers during calculation. Try with simple examples first.
JW
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-09-07 10:38 PM
I tried both http://www.sunshine2k.de/coding/javascript/crc/crc_js.html and https://crccalc.com/. These two match well.
Then I tried various Input/Output Reflect (Reverse or Non-reverse), Initial value(0x0 or 0xFF). So far, none match the result from above sites.
Maybe only ST guys with internal info can solve the puzzle. It's from their example, wonder how they verified the result.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-09-07 11:27 PM
The screenshot I gave above matches the value you said in initial post comes from STM32.
Did you observe the CRC registers during calculation? Show us, what you've seen, for a simple example.
JW
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-09-08 11:21 AM
Thanks to the OPs who viewed this thread, especially @waclawek.jan and @TDK. Just to update in case it can be helpful to anyone may run into it.
I dug a little more in the Calculate_CRC() of the example, seems the original code trying to use the 32B capacity as much as possible even for CRC8, should be more efficiently if possible, but it's over my head and didn't work for me.
With a minor mods to just use 8B data feed, now the result matches the other calculator.