Skip to main content
DAlbe.3
Associate III
May 24, 2024 12:41 AM UTC
Solved

STM32G030 readout protection level 1 (errata 2.2.3) POR lockup if boot select via BOOT0 pin enabled

EDITED:
Resolved, but leaving here for the next person who stumbles into this issue.
I'm using the STM32G030K6 and encountered two issues:

  1. Errata 2.2.3 - which correctly describes a serious issue when using readout protection level 1: if nBOOT_SEL is not set in the option bits, the uC will often fail to boot and even a hard reset will not recover, only a power cycle.  The errata correctly describes a workaround: set nBOOT_SEL in the option bits (removes the option to force entry to the bootloader by tying the BOOT0 pin high).
  2. Access to OTP memory is not protected by readout protection level 1.
    This is expected behavior since SystemMemory is not protected by RDP level 1, but it is unfortunate given that OTP is the perfect place to store device-specific persistent data like serial numbers, encryption keys, etc. This is particularly true on devices with limited flash where allocating a separate sector may be painful. Perhaps in a future version of the component, ST will consider protecting OTP as well as the code space.

The rest of this thread is obsolete, it was the result of a failed component where I could not set the nBOOT_SEL bit successfully.  Many thanks to @waclawek.jan for all of the patience and help!

This topic has been closed for replies.
waclawek.jan
waclawek.janBest answer
Super User
May 24, 2024 2:15 PM UTC

> The package I'm using (LQFP32 - sorry, that's the K6 variant, not F6 as I'd originally posted) does not have separate VBAT and VDD pins

That does not really matter; the problem is with VBAT reaching a specific low voltage, regardless of what VDD does (as long as VDD is not above the "VDD brownout/POR" level, in which case VBAT is disconnected internally).

> and even if it did, any condition that does not clear with a hard reset should be viewed as a critical failure.

Yes it is; that's why it's in the errata.

> This *never* happens with RDP set to level 0; the product had been in development for months, always using RDP level 0 and we'd never seen this issue..

I hear you; but, during development, did you try to fade the VDD down to the problematic levels?

Or, now, having encountered the problem, did you try to remove RDP1, reprogram without RDP, and fade VDD? Okay I overlooked "does not ever happen if RDP is set back to level 0"

Btw. do you have code there which explicitly tests RDP (or any other bits from the option bytes)?

> I added code (very early in boot) to reset the backup power domain if the reset reason indicated power:

Are you sure that code does reset the backup power domain? Do you have backup domain access enabled in PWR previously (which in turn requires PWR to have clock enabled in RCC)?

 

Note that I don't claim this is certainly the source of your problem; but I see this as a possibility which may act through unexpected relationships.

 

An interesting exercise might be toggling a GPIO output at strategic points of the code startup, and then observing it on the problematic device.

JW

22 replies

DAlbe.3
DAlbe.3Author
Associate III
May 24, 2024 6:35 PM UTC

Progress: I swapped out the chip on the unit I've been having trouble setting the nBOOT_SEL bit and now that piece is working!  So I now have a unit configured with RDP level=1 and the BOOT option bit set correctly and so far I have not been able to reproduce the failure-to-boot with this configuration.  I'll update again if I reproduce it, but I think my problem was a failed part...thank you so much for the help @waclawek.jan.

I think the only thing worth noting then is that with RDP level 1, the OTP memory is still accessible for read via STLink

DAlbe3_0-1716575681160.png

DAlbe3_1-1716575837935.png

 

I will change the title of this thread to indicate that and I'll test on a few more units; if I can't reproduce the problem, I'll mark this closed.

waclawek.jan
Super User
May 25, 2024 9:47 AM UTC

Thanks for coming back with the solution. Please click on "Accept as solution" in that post so that the thread is marked as solved.

I wonder what caused the problematic nBOOT_SEL option bit. It can't be wear, as the inverted value is always matching the "straight" one, even after the surprising change during powerdown.

I have doubts about the OTP lock and start a separate thread to ask ST for comment, as it is a separate problem from this (btw. have a look at the table you've posted, in the newest revision of RM0454 - it differs exactly in this detail).

JW

Jocelyn RICARD
ST Employee
May 27, 2024 12:06 PM UTC

Hello @DAlbe.3 ,

I confirm OTP value can be read in RDP1 on STM32G0. I checked on few different G0 part numbers.

I will raise the point internally to get the RM fixed.

Best regards

Jocelyn

DAlbe.3
DAlbe.3Author
Associate III
May 27, 2024 7:26 PM UTC

Thank you Jocelyn. There are probably multiple documents that need correction; for example, see slide 8 here:
https://www.st.com/content/ccc/resource/training/technical/product_training/group0/68/e5/5c/b5/40/10/43/22/STM32G0-Security-Memories-Protections-MEMPROTECT/files/STM32G0-Security-Memories-Protections-MEMPROTECT.pdf/_jcr_content/translations/en.STM32G0-Security-Memories-Protections-MEMPROTECT.pdf

If there is ever a silicon revision of the STM32G0, I think it would be better to make the silicon match the documentation and protect OTP when RDP is set to readout protection level 1.  I can think of very few cases where the current behavior is what developers would desire or expect.  OTP would be dramatically more useful if you could secure data stored there.

Jocelyn RICARD
ST Employee
May 28, 2024 9:52 AM UTC

Hello @DAlbe.3 ,

I agree there is an issue in the documentation.

Now regarding the actual protection of OTP value, I don't think this is an issue.

OTP are One Time Programmable and are not erased on RDP regression.

So, protecting OTP while in RDP1 does not bring you any OTP confidentiality protection as long as you can regress the device to RDP0 and read the OTP in clear.

Here, OTP purpose is to ensure immutability of the data, not confidentiality 

If you need this confidentiality, you must use RDP2. In that case, it you need to update the firmware, you will need a secure boot and loader in user flash to make sure a fake firmware cannot be installed.

Best regards

Jocelyn

waclawek.jan
Super User
May 27, 2024 12:51 PM UTC

Thanks, @Jocelyn RICARD .

JW

Explorer
Oct 1, 2024 8:47 AM UTC

Thank you! I've encountered the very same problem with STM32G030F6P6. Setting nBOOT_SEL option works for me.

I would like to add some hardware details about the issue I encountered. This problem is highly related to the power supply. On my PCB, there is a 470uF capacitor. When the system powers on, if this capacitor is fully discharged, the STM32 fails to start. However, if the capacitor has a small residual voltage (> 0.xV), the STM32 starts normally.

I used an oscilloscope to check the VCC voltage rise curves in both cases, and I didn’t find obvious differences.