2019-09-04 6:47 AM
I tried the SBSFU examples (did not change any code) on a NUCLEO-L476RG board and it worked fine. Now I can not use STM32CubeProgrammer to connect the board. Is there any way to download a new firmware ( I mean, a firmware to replace the SBSFU firmware) to the board again? So that I can use this board for other projects.
The configuration of the SBSFU is:
/*#define SECBOOT_DISABLE_SECURITY_IPS*/
/*#define SFU_FINAL_SECURE_LOCK_ENABLE */
#define SFU_DEBUG_MODE
/*#define SFU_FWIMG_BLOCK_ON_ABNORMAL_ERRORS_MODE*/
#define SECBOOT_OB_DEV_MODE
Thanks!
2019-09-04 6:59 AM
Hello Zoey,
by default, the SBSFU will apply all the protections available.
One of these protections is the RDP level 1 (as long as you didn't uncomment the final secure lock enable).
Also, the GPIOs used for the SWD connection were set to another alternate function.
With the Readout Protection level, you can still attach to the target but you need to set the mode to "Under reset" in the Cube programmer.
Once connected, go to option bytes and set RDP level to 0xAA (RDP level 0)
This will provoke a mass erase and take you back to a clean device.
Another way would be to set the BOOT0 pin to 1 and to connect to the system bootloader through DFU or USART.
The STM32CubeProgrammer is able to handle these communication links and will allow you to do the RDP regression.
Best regards
Jocelyn
2019-09-09 7:55 AM
Thanks very much, Jocelyn.
I tried to set the mode to "Under reset" in the Cube programmer and with different reset modes (software reset, hardware reset, core reset), it failed to connect and showed the following messages
16:45:52 : STM32CubeProgrammer API v2.1.0
16:45:52 : ST-LINK error (DEV_CONNECT_ERR)
16:46:25 : ST-LINK error (DEV_USB_COMM_ERR)
16:46:25 : Error: Problem occured while trying to connect
16:46:53 : ST-LINK error (DEV_USB_COMM_ERR)
16:46:53 : Error: Problem occured while trying to connect
16:47:06 : ST-LINK error (DEV_USB_COMM_ERR)
16:47:06 : Error: Problem occured while trying to connect
I will try the second way and see.
2019-09-10 12:54 AM
After setting the BOOT0 pin to 1 and connecting to the system bootloader USART, I could set the RDP level to 0xAA (RDP level 0). However, I could not erase the chip.
09:47:59 : ST-LINK FW : V2J31M21
09:47:59 : Voltage : 3.28V
09:47:59 : SWD freq : 4000 KHz
09:47:59 : Connect mode: Under Reset
09:47:59 : Reset mode : Hardware reset
09:47:59 : Device ID : 0x415
09:47:59 : UPLOADING OPTION BYTES DATA ...
09:47:59 : Bank : 0x00
09:47:59 : Address : 0x40022020
09:47:59 : Size : 20 Bytes
09:47:59 : Bank : 0x01
09:47:59 : Address : 0x40022044
09:47:59 : Size : 16 Bytes
09:47:59 : UPLOADING ...
09:47:59 : Size : 1024 Bytes
09:47:59 : Address : 0x8000000
09:47:59 : Read progress:
09:47:59 : Data read successfully
09:47:59 : Time elapsed during the read operation is: 00:00:00.008
09:48:04 : MASS ERASE ...
09:48:04 : Error: Mass erase operation failed.Please verify flash protection
How can I make mass erase work? Thanks!
2019-09-10 8:04 AM
Hello Zoey,
One first thing to do would be to update the stlink firmware.
When connected with STM32CubeProgrammer click on firmware upgrade button and follow instructions
Then please launch the following command:
STM32_Programmer_CLI.exe -c port=SWD -ob displ
and just copy paste here the option byte contents.
I will have a look and tell you what to do.
Best regards
Jocelyn