Skip to main content
s2000
Associate
May 7, 2025
Solved

HRTIM Triggering ADC

  • May 7, 2025
  • 1 reply
  • 814 views

Hi,

I am currently working with the STM32F334 and STM32G474 microcontrollers, and I have a couple of technical questions that require deeper insight into how the HRTIM (High-Resolution Timer) operates in these devices.


Q1. Can HRTIM generate a high-resolution variable-frequency waveform?
From my own testing, it appears yes, but I would like to confirm this officially. To clarify what I mean: suppose I am designing a resonant converter operating at 1 MHz. In the STM32F334, the HRTIM supports an effective edge resolution of ~217 ps, equivalent to a virtual clock of 4.608 GHz. This means the period register value for 1 MHz would be 4.608GHz/ 1MHz = 4608. Now, if I reduce the period by just one count 4.608GHz / 4607 = 1000217MHz This implies a frequency resolution of ~217 Hz. However, if high-resolution control were not supported for the period register, the period would instead be based on the timer base clock 144 MHz / 143  = 1.006993MHz. That would mean a frequency step of ~6993 Hz, much coarser than in the high-resolution case. In my practical testing, the frequency resolution I observed matched the 217 Hz scenario, suggesting that HRTIM does indeed support high-resolution period updates, or at least, simulates them through sub-tick edge positioning. Can you confirm whether HRTIM truly supports high-resolution frequency adjustment through fractional edge interpolation of the period?


Q2. If a HRTIM compare register triggers an ADC conversion, does the trigger also maintain 217 ps resolution?

In the above scenario, if a compare register is configured to trigger an ADC start of conversion, does this signal also carry sub-nanosecond resolution (~217 ps), or is it internally synchronized with the 72 MHz system clock, losing the high-resolution timing? I understand that the ADC requires at least 1.5 cycles for sampling and 12.5 cycles for conversion, and that its internal operations are governed by the ADC clock. However, my question is about the precision of the triggering edge, particularly whether the start-of-conversion (SOC) signal benefits from the high-resolution HRTIM output. It seems to me that high-resolution triggering of the ADC may not have a significant impact, since regardless of the SOC precision, the end of the sampling phase is ultimately synchronized to the 72 MHz ADC clock.

Best answer by ST_Sophia

Hello, 

Please find below a couple of feedback:

Q1. "Can HRTIM generate a high-resolution variable-frequency waveform ?"


R1: Yes, HRTIM truly supports high-resolution frequency adjustment. STM32G4 for instance contains a DLL running at 5.44Ghz for this purpose:
rm0440-stm32g4-series-advanced-armbased-32bit-mcus-stmicroelectronics.pdf:
"High-resolution timing units
– 184 ps resolution, compensated against voltage and temperature variations
– High-resolution available on all outputs, possibility to adjust duty-cycle, frequency 
and pulse width in triggered one-pulse mode"

 

Q2. "If a HRTIM compare register triggers an ADC conversion, does the trigger also maintain 217ps resolution?
It seems to me that high-resolution triggering of the ADC may not have a significant impact, since regardless of the SOC precision, the end of the sampling phase is ultimately synchronized to the 72 MHz ADC clock."

 

R2: Indeed, high resolution triggers when transferred to ADC won't be useful, since ADC is running at its own frequency which is not HR, and regarding sampling/conversion constraints, we won't get a significant advantage by making it HR.

 

Best regards.

1 reply

ST_Sophia
ST_SophiaBest answer
ST Employee
May 13, 2025

Hello, 

Please find below a couple of feedback:

Q1. "Can HRTIM generate a high-resolution variable-frequency waveform ?"


R1: Yes, HRTIM truly supports high-resolution frequency adjustment. STM32G4 for instance contains a DLL running at 5.44Ghz for this purpose:
rm0440-stm32g4-series-advanced-armbased-32bit-mcus-stmicroelectronics.pdf:
"High-resolution timing units
– 184 ps resolution, compensated against voltage and temperature variations
– High-resolution available on all outputs, possibility to adjust duty-cycle, frequency 
and pulse width in triggered one-pulse mode"

 

Q2. "If a HRTIM compare register triggers an ADC conversion, does the trigger also maintain 217ps resolution?
It seems to me that high-resolution triggering of the ADC may not have a significant impact, since regardless of the SOC precision, the end of the sampling phase is ultimately synchronized to the 72 MHz ADC clock."

 

R2: Indeed, high resolution triggers when transferred to ADC won't be useful, since ADC is running at its own frequency which is not HR, and regarding sampling/conversion constraints, we won't get a significant advantage by making it HR.

 

Best regards.

s2000
s2000Author
Associate
May 13, 2025

Thanks, Yassine, for your response, it was very insightful. I've spent quite a bit of time working with various microcontrollers with high-resolution timer, and it's interesting to see that ST is one of the few vendors capable of generating high-resolution-variable-frequency signals. Many competitors lack this capability, and only can make HR duty cycle, which may be why they label it as HRPWM. I’ve actually suggested to ST that they emphasize and promote this feature more, as it makes a significant difference when it comes to variable-frequency control in resonant converters.

ST_Sophia
ST Employee
May 13, 2025

Thank you, Sayed Amir, for your feedback, 

I will report it internally to my colleagues responsible of this feature,

Best regards.