Skip to main content
Associate II
May 8, 2025
Solved

STM32H747i-DISCO - Added initially U-Boot support

  • May 8, 2025
  • 1 reply
  • 413 views

Hi ST community members!

 

For a long time ago with another nick (but lost the account access), I have wanted to add U-Boot support for this board. Now I have done this but not released a patch series yet (only on my local Git repo) in the U-Boot mailing list. Also must do some tests on real hardware.

 

Short question:

Does somebody need support for this board or is it useless? I know the board has less RAM, but some ST maintainers on the U-Boot list where interested in the past. But unfortunately I haven't finally done this, because of an illness. Also when it's useless for other users, it was a fun project for me. :)

This topic has been closed for replies.
Best answer by krotti42

Tests succeed  (runs now):

U-Boot 2025.07-rc1-00141-g48db49b0977c-dirty (May 08 2025 - 19:22:08 +0200)

Model: STMicroelectronics STM32H747i-Discovery board
DRAM: 32 MiB
Core: 30 devices, 16 uclasses, devicetree: separate
MMC: STM32 SD/MMC: 0
Loading Environment from nowhere... OK
In: serial@40011000
Out: serial@40011000
Err: serial@40011000
Hit SPACE in 30 seconds to stop autoboot.
U-Boot >

Had must add some SoC specific code, because I used the preexisting source from board STM32H743-DISCO. And without this SoC specific code a had a deadlock from the board, because of the missing early initialization from the PWR register from the SoC.

 

Also I have must changed the stm32h7-pinctrl device tree to get a serial output. Was mapped to other pins for USART1.

1 reply

krotti42AuthorBest answer
Associate II
May 8, 2025

Tests succeed  (runs now):

U-Boot 2025.07-rc1-00141-g48db49b0977c-dirty (May 08 2025 - 19:22:08 +0200)

Model: STMicroelectronics STM32H747i-Discovery board
DRAM: 32 MiB
Core: 30 devices, 16 uclasses, devicetree: separate
MMC: STM32 SD/MMC: 0
Loading Environment from nowhere... OK
In: serial@40011000
Out: serial@40011000
Err: serial@40011000
Hit SPACE in 30 seconds to stop autoboot.
U-Boot >

Had must add some SoC specific code, because I used the preexisting source from board STM32H743-DISCO. And without this SoC specific code a had a deadlock from the board, because of the missing early initialization from the PWR register from the SoC.

 

Also I have must changed the stm32h7-pinctrl device tree to get a serial output. Was mapped to other pins for USART1.