cancel
Showing results for 
Search instead for 
Did you mean: 

XNUCLEOBNRG2A1 and NUCLEOU575

IVent.1
Senior

Hi,

I picked up a X-NUCLEO-BNRG2A1, and I am trying to communicate with it through a Nucleo-U575 Board. I basically generated a project template through CubeMX for the STM32U575 and included the BlueNRG-2 (X-CUBE-BLE2) Pack to include Bluetooth HCL/ACI APIs along with the project template. These are some images from cubeide. The project doesn't work...when the flow enters in MX_BlueNRG_2_Init,  hci_send_req function
returns BLE_STATUS_TIMEOUT. D7 pin and the pin #5 of the J12 on the X-NUCLEOBNRG2A1
expansion board are bridged. Is there something else to do in order to make all works together?thank you

Isabella

3 REPLIES 3
FBL
ST Employee

Hello @IVent.1 

 

It could be required to bridge D13 and D3 pins to set correctly SPI SCK.

 

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.


I'm out of offce with limited access to my emails.
Happy New Year!

Also with D3 and D13 connected, hci_send_req function returns BLE_STATUS_TIMEOUT.

IVent.1
Senior

No other suggestions, please? thank you.