cancel
Showing results for 
Search instead for 
Did you mean: 

STM32G4: Wrong description of HRTIM_ADCxR registers in RM0440 Rev 9

simountain
Associate II

If I am correct, the descriptions of
 - HRTIM_ADC2R
   -  Bit 22
 - HRTIM_ADC3R
   - Bit 19
   - Bit 13
 - HRTIM_ADC3R
   - Bit 22
   - Bit 13
   - Bit 10
   - Bit 5
   - Bit 4
   - Bit 0
are not correct in the RM.

They all describe trigger event generation but the trigger output in all these seem wrong:
E.g.: HRTIM_ADC2R, Bit 22,
Original Text: "This bit enables the generation of an ADC trigger upon timer C reset and roll-over event, on ADC trigger 1 output."
It should be: "This bit enables the generation of an ADC trigger upon timer C reset and roll-over event, on ADC trigger 2 output."

Also, I want to ask, if this forum is the right place to give feedback on documentation issues?

Best Simon

1 REPLY 1
Imen.D
ST Employee

Hello @simountain and welcome to the Community,

Thank you for bringing this issue to our attention.

An internal ticket number 224817 is submitted in order to fix this. 

 

Also, I want to ask, if this forum is the right place to give feedback on documentation issues?


Yes, this is the right place to share this kind of feedback and report issues. Please feel free to share them with us here.

Thank you for your contributions.

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen