cancel
Showing results for 
Search instead for 
Did you mean: 

wrong ADC DMA Continous conversion data order

Gaston
Senior

Hi,

I cannot understand acquired ADC data order using this configuration on a STM32G030C6 device:

Gaston_0-1716916097772.png

I want to acquire 9 input channels + 2 internal channels (Temperature Sensor + Vbat). Continuous mode w/ Circular DMA

Gaston_1-1716916217782.png

Here's my Initialization routine

 

static uint32_t adc_values[11];

HAL_ADCEx_Calibration_Start(&hadc1);
// DMA continous requests: ENABLED
HAL_ADC_Start_DMA(&hadc1, adc_values, 11);

 

Everything works as expected except the channels order.

  • adc_values[0] ---> OK
  • adc_values[1] ---> OK
  • adc_values[2] ---> OK
  • adc_values[3] ---> OK
  • adc_values[4] ---> OK
  • adc_values[5] ---> KO This should be (afaik) the internal temperature sensor channel but I see the IN8 adc value.
  • adc_values[6] ---> KO This should be (afaik) the IN8 channel but I see the IN9 channel.
  • adc_values[7] ---> KO Does not match either.
  • adc_values[8] ---> KO Does not match either.
  • adc_values[9] ---> KO Does not match either.
  • adc_values[10] ---> KO Does not match either.

Does anyone know what the problem is?
I'm not able to find any example with similar configuration.

Thanks in advance,
Gaston

 

1 ACCEPTED SOLUTION

Accepted Solutions

Oh, ok , on G030 ...

AScha3_0-1716925031305.png

So check, whats the "ch numbers" ...this is the sequence then.

see rm...

AScha3_1-1716925218551.png

 

If you feel a post has answered your question, please click "Accept as Solution".

View solution in original post

4 REPLIES 4
AScha.3
Chief II

Hi,

the sequence depends on the Rank numbers - what you set ? 

On every Rank you can choose, which channel is it , to convert. So you decide about the sequence !

see:

AScha3_0-1716922962198.png

I set 3 conversions, but 2. is temp channel...because i choose it for Rank 2.

If you feel a post has answered your question, please click "Accept as Solution".

Thank you for replying. I know this but I see no way to select Rank numbers in this ADC configuration. Notes that Sequencer is set to not fully configurable as I need IN15 and IN16 input channels.

Oh, ok , on G030 ...

AScha3_0-1716925031305.png

So check, whats the "ch numbers" ...this is the sequence then.

see rm...

AScha3_1-1716925218551.png

 

If you feel a post has answered your question, please click "Accept as Solution".

Blessed RM 🙏 I should have checked it before raising the question. Now it makes sense.

Thank you very much AScha.3!

Gaston