cancel
Showing results for 
Search instead for 
Did you mean: 

Write and read using Flash memory on STM32F7xx (24 sectors)

ZYagu.1
Associate II

I've got the following structure to write to memory:

```

#define FLASH_CONFIG_START_ADDR ((uint32_t) 0x080E0000)

#define FLASH_CONFIG_END_ADDR ((uint32_t) 0x080E0040)

union NVRAM {

Config_t config;

uint8_t data[512];

} DevNVRAM;

```

I've used this code for writing to memory

```

uint32_t l_address = FLASH_CONFIG_START_ADDR;

uint8_t l_index = 0x00;

l_address = FLASH_CONFIG_START_ADDR;

HAL_FLASH_Unlock();

FLASH_Erase_Sector(FLASH_SECTOR_11, VOLTAGE_RANGE_1);

while (l_address < FLASH_CONFIG_END_ADDR)

if (HAL_FLASH_Program(FLASH_TYPEPROGRAM_BYTE, l_address,

DevNVRAM.data[l_index]) == HAL_OK) {

l_index += 1;

l_address += 1;

}

HAL_FLASH_Lock();

```

and then I simply read from the same block of memory.

```

l_address = FLASH_CONFIG_START_ADDR;

l_index = 0x00;

while (l_address < FLASH_CONFIG_END_ADDR) {

DevNVRAM.data[l_index] = *(uint8_t*) l_address;

l_index += 1;

l_address += 1;

}

```

The problem is the following, after I have read the whole sector, data becomes different, in particular, it is filled with zeros. What is the problem with code?

P.S. How can I get first address of memory blovk in the sector without hard-coddding?

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
ZYagu.1
Associate II

The problem was in address declaration. it is actually 0x81C000(viewd in st-link utility)

View solution in original post

14 REPLIES 14
waclawek.jan
Super User

Cache-related?

Which STM32 in particular?

How is single-bank/dual-bank set?

JW

Is the data you want to write 64 or 512 bytes long?

Why write as bytes, doesn't this need to be words or double words?​

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

STM32F767ZI dual-bank

Actual size of data is 14 bytes, FLASH_TYPEPROGRAM_BYTE is allowed according to hal_flash.h

TDK
Super User

Are you using the union properly and not overwriting data? Does reading the memory in the debugger match what you're reading in your code?

If you feel a post has answered your question, please click "Accept as Solution".

I am using debugger and memory monitoring, looks like writing data to memory is not working​ since union is correct(also have checked with debugger)

TDK
Super User

You shouldn't be calling FLASH_Erase_Sector directly. You should be calling HAL_FLASHEx_Erase. There are other things you're missing as a result.

If you feel a post has answered your question, please click "Accept as Solution".

I have changed the code:

```

static FLASH_EraseInitTypeDef EraseInitStruct;

EraseInitStruct.TypeErase = FLASH_TYPEERASE_SECTORS;

EraseInitStruct.Sector = FLASH_CONFIG_START_ADDR;

EraseInitStruct.NbSectors = 0x01;

HAL_FLASH_Unlock();

HAL_FLASHEx_Erase(&EraseInitStruct, &l_error);

```

Now i have this instead of: FLASH_Erase_Sector(FLASH_SECTOR_11, VOLTAGE_RANGE_1);

Unfortunately, this didn't fix the problem, I suppose the problem is with wirting to memory.

TDK
Super User

> EraseInitStruct.Sector = FLASH_CONFIG_START_ADDR;

This is not a sector value.

Monitor the return values from HAL.

If you feel a post has answered your question, please click "Accept as Solution".