cancel
Showing results for 
Search instead for 
Did you mean: 

Write and read using Flash memory on STM32F7xx (24 sectors)

ZYagu.1
Associate II

I've got the following structure to write to memory:

```

#define FLASH_CONFIG_START_ADDR ((uint32_t) 0x080E0000)

#define FLASH_CONFIG_END_ADDR ((uint32_t) 0x080E0040)

union NVRAM {

Config_t config;

uint8_t data[512];

} DevNVRAM;

```

I've used this code for writing to memory

```

uint32_t l_address = FLASH_CONFIG_START_ADDR;

uint8_t l_index = 0x00;

l_address = FLASH_CONFIG_START_ADDR;

HAL_FLASH_Unlock();

FLASH_Erase_Sector(FLASH_SECTOR_11, VOLTAGE_RANGE_1);

while (l_address < FLASH_CONFIG_END_ADDR)

if (HAL_FLASH_Program(FLASH_TYPEPROGRAM_BYTE, l_address,

DevNVRAM.data[l_index]) == HAL_OK) {

l_index += 1;

l_address += 1;

}

HAL_FLASH_Lock();

```

and then I simply read from the same block of memory.

```

l_address = FLASH_CONFIG_START_ADDR;

l_index = 0x00;

while (l_address < FLASH_CONFIG_END_ADDR) {

DevNVRAM.data[l_index] = *(uint8_t*) l_address;

l_index += 1;

l_address += 1;

}

```

The problem is the following, after I have read the whole sector, data becomes different, in particular, it is filled with zeros. What is the problem with code?

P.S. How can I get first address of memory blovk in the sector without hard-coddding?

This discussion is locked. Please start a new topic to ask your question.
14 REPLIES 14
Piranha
Chief II

By default the FLASH memory is configured as write-through. Because of that cache cleaning is not necessary, but after erasing or programming still a cache invalidation needs to be done on the corresponding FLASH memory addresses. For data memory use SCB_InvalidateDCache_by_Addr() to invalidate D-cache.

I have tried EraseInitStruct.Sector = FLASH_SECTOR_11; but this didn't help.

I have added SCB_InvalidateDCache_by_Addr(FLASH_CONFIG_START_ADDR, FLASH_CONFIG_END_ADDR - FLASH_CONFIG_START_ADDR);

After Locking Flash. Still didn't fix the problem.

I actually think that it should work since this function is declared in stm32f7xx_hal_flash.c file

ZYagu.1
Associate II

The problem was in address declaration. it is actually 0x81C000(viewd in st-link utility)