How to unlock STM32F103C8T6 ?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2021-06-01 4:52 AM
Hello,
I have several modules with STM32F103C8T6 (called Blue Pills). But I cannot get them to run
the programs.
I can freely write or read flash memory with stm32cubeprogrammer, but there is always warning (even when I want to start the program), that the core is locked.
How can I unlock the MCU?
Here is the programmer's log :
13:49:30:294 : STLinkUSBDriver.dll loaded
13:49:30:295 : STLinkUSBDriver.dll loaded
13:49:30:295 : ST-LINK SN : 066EFF564948897767014518
13:49:30:295 : ST-LINK FW : V2J37M27
13:49:30:296 : Board : NUCLEO-L053R8
13:49:30:297 : Voltage : 3.25V
13:49:30:309 : SWD freq : 4000 KHz
13:49:30:310 : Connect mode: Normal
13:49:30:310 : Reset mode : Software reset
13:49:30:317 : Device ID : 0x410
13:49:30:321 : Revision ID : Rev X
13:49:30:342 : flash loader C:\Program Files\STMicroelectronics\STM32Cube\STM32CubeProgrammer\bin/FlashLoader/0x410.stldr is loaded
13:49:30:343 : Reading data...
13:49:30:344 : r ap 0 @0x1FFFF7E0 0x00000004 bytes Data 0xFFFF0040
13:49:30:520 : UPLOADING OPTION BYTES DATA ...
13:49:30:520 : Bank : 0x00
13:49:30:520 : Address : 0x4002201c
13:49:30:520 : Size : 8 Bytes
13:49:30:521 : Reading data...
13:49:30:521 : r ap 0 @0x4002201C 0x00000008 bytes Data 0x03FFFFFC
13:49:30:521 : Bank : 0x01
13:49:30:521 : Address : 0x1ffff800
13:49:30:521 : Size : 16 Bytes
13:49:30:522 : Reading data...
13:49:30:522 : r ap 0 @0x1FFFF800 0x00000010 bytes Data 0x00FF5AA5
13:49:30:522 : UPLOADING OPTION BYTES DATA ...
13:49:30:522 : Bank : 0x00
13:49:30:522 : Address : 0x4002201c
13:49:30:522 : Size : 8 Bytes
13:49:30:523 : Reading data...
13:49:30:523 : r ap 0 @0x4002201C 0x00000008 bytes Data 0x03FFFFFC
13:49:30:523 : Bank : 0x01
13:49:30:523 : Address : 0x1ffff800
13:49:30:523 : Size : 16 Bytes
13:49:30:523 : Reading data...
13:49:30:523 : r ap 0 @0x1FFFF800 0x00000010 bytes Data 0x00FF5AA5
13:49:30:524 : UPLOADING ...
13:49:30:524 : Size : 1024 Bytes
13:49:30:524 : Address : 0x8000000
13:49:30:524 : Read progress:
13:49:30:524 : Reading data...
13:49:30:525 : r ap 0 @0x08000000 0x00000400 bytes Data 0x20005000
13:49:30:526 : Data read successfully
13:49:30:526 : Time elapsed during the read operation is: 00:00:00.007
13:49:42:867 : Memory Programming ...
13:49:42:868 : Opening and parsing file: hid_generic_pc13.bin
13:49:42:871 : File : hid_generic_pc13.bin
13:49:42:871 : Size : 1976 Bytes
13:49:42:871 : Address : 0x08000000
13:49:42:872 : Erasing memory corresponding to segment 0:
13:49:42:882 : Memory erase...
13:49:42:897 : Erasing internal memory sectors [0 1]
13:49:42:897 : Init flashloader...
13:49:42:913 : Loader sector erase...
13:49:42:942 : Download in Progress:
13:49:42:943 : Size : 1976 Bytes
13:49:42:943 : Address : 0x08000000
13:49:42:943 : Buffer program...
13:49:42:961 : Loader write range...
13:49:42:976 : Init flashloader...
13:49:43:038 : Segment[0] downloaded successfully
13:49:43:039 : File download complete
13:49:43:061 : Time elapsed during download operation: 00:00:00.170
13:49:43:062 : Verifying ...
13:49:43:062 : Read progress:
13:49:43:062 : Reading data...
13:49:43:069 : Reading data...
13:49:43:070 : Download verified successfully
13:49:43:097 : RUNNING Program ...
13:49:43:097 : Address: : 0x08000000
13:49:43:097 : Warning: The core is locked up
13:49:43:120 : Start operation achieved successfully
- Labels:
-
Flash
-
STM32F1 Series
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2021-06-01 5:11 AM
Have you tried doing mass earase with stm32cubeprogrammer?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2021-06-06 3:54 AM
Yes, it all works without problem.
I do erase whole chip, flash the program but I'm not sure whether I should do something with Boot jumpers and when...
Somewhere it says, that I should change Boot jumpers to "run from flash" before disconnecting.
Have tried several scenarios, but none works...
But according to programmer, I can write and read Flash properly. I just reports mentioned warning all the time, when it tries to run the program.
Any hint ?