cancel
Showing results for 
Search instead for 
Did you mean: 

World’s highest performance Cortex™-M microcontroller

Nickname12657_O
Associate III
Posted on September 22, 2011 at 13:00

http://www.st.com/internet/mcu/subclass/1521.jsp?WT.ac=p2_bn_sep11_stm32f4series

The STM32 F4 series is the world�s highest performance Cortex�-M microcontroller � 168 MHz (Cortex-M4 with FPU) CPU, 210 DMIPS, 363 Coremark score;

The STM32 F4 is available now and ST will be distributing STM32 F4 Discovery Kits at the Embedded Systems Conference in Boston, Sept 27-28;

The STM32 F4 series extends the STM32 portfolio and now has 250+ compatible devices already in production, including the F1 series, F2 series and ultra-low-power L1 series

The STM32 F4 reinforces ST�s leadership in Cortex-M microcontrollers, with 45% world market share by units (cumulated 2007-Q1 2011 period according to ARM Cortex-M unit shipments reporting)

Continue Releasing your Creativity with our STM32 !

Cheers,

STOne-32.

http://www.st.com/internet/evalboard/product/252419.jsp

#rest-of-world
20 REPLIES 20
Andrew Neil
Evangelist III
Posted on September 24, 2011 at 10:54

''Continue Releasing your Creativity with our STM32 !''

 

 

But only, apparently, if you're in North America!

:(

I note that free Discovery kits are available - but only to

North America!

:(

 

 

Come on, ST - there's more to the world than just North America!
dmatheis2
Associate II
Posted on September 26, 2011 at 10:24

Yes, give some boards also to Europe, especially to the students!

Andrew Neil
Evangelist III
Posted on September 26, 2011 at 15:03

''give some boards also to Europe, especially to the students!''

 

 

No - me first! Me! Meeeeeeeeeee!!!

😉

emalund
Associate III
Posted on September 26, 2011 at 20:32

Come on, ST - there's more to the world than just North America!

 

 

well, ST is hjeadquartered in Europe, I doubt they do not know that 🙂

Erik
root
Associate II
Posted on September 27, 2011 at 07:39

Hello,

I thought it would be interesting to say that Altium already released TASKING for ARM v4.0r1 that works with the STM32F4 series and with ST Link V2 (previously only ST Link V1). Works flawlessly for me.

About ST Micro, at first it was a French company, is it still one (just kidding)?

We also have a few engineers in Europe ... Of course a discovery kit would be welcome, but I'm mainly looking for a TQFP-64 STM32F4 to put on one of my boards (designed for STM32F205Rx), and price/availability.

Thomas.
Andrew Neil
Evangelist III
Posted on September 27, 2011 at 07:58

''well, ST is hjeadquartered in Europe, I doubt they do not know that :)''

Which makes it particularly ironic that they shoud be acting like a North American corporation, and ignoring the rest of the world!

:(
emalund
Associate III
Posted on September 27, 2011 at 14:56

someone once said: ''there are 3 ways to do things, the right way, the wrong way and the French way'' 🙂

Erik

Posted on September 27, 2011 at 17:03

But isn't this website hosted by ST's North American unit, and probably semi autonomous? The world HQ is in Switzerland, which as I recall isn't a member of the EU, the populous actually afforded a referendum on the issue.

Perhaps the flak would be better directed at the European sales/marketing arm, or through your local representatives/distributors/FAEs.

NA sales/marketing were around last month talking about the M0/M4 roadmaps.

http://www.st.com/internet/com/press_release/p3029.jsp

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
emalund
Associate III
Posted on September 27, 2011 at 18:16

no, but it IS in Europe

Erik

Posted on September 27, 2011 at 19:03

no, but it IS in Europe

Indeed in/within Europe but not in the Union, in the same way Quebec is in Canada, different rules apply. You'd think NA ST would have manuals readily available in French, and equally prominent.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..