Skip to main content
Associate
March 28, 2024
Solved

Importance of Rext Resistor in STM32 external Crystal Oscillator

  • March 28, 2024
  • 1 reply
  • 2024 views

Hello ST community,

I'm currently working on a circuit utilizing an ATS240C-E Crystal with a 22pF capacitor for an STM32 microcontroller. I'm curious about the necessity and implications of including a Rext resistor in the output of the crystal oscillator. Could anyone shed light on whether the Rext resistor is necessary for STM32 microcontrollers? Furthermore, I'd like to understand how its presence or absence affects the performance, stability, and functionality of the oscillator, particularly in noisy and EMI conditions.

If anyone has insights or experiences to share regarding this matter, I would greatly appreciate it.

Thank you in advance for your assistance.

This topic has been closed for replies.
Best answer by mƎALLEm

Hello,

Refer to the AN2867 "Guidelines for oscillator design on STM8AF/AL/S, and STM32 MCUs/MPUs"

Specifically the section: 3.5 Drive level and external resistor calculation / 3.5.3 Calculating the external resistor.

Hope it does answer your question.

1 reply

mƎALLEm
mƎALLEmBest answer
ST Technical Moderator
March 28, 2024

Hello,

Refer to the AN2867 "Guidelines for oscillator design on STM8AF/AL/S, and STM32 MCUs/MPUs"

Specifically the section: 3.5 Drive level and external resistor calculation / 3.5.3 Calculating the external resistor.

Hope it does answer your question.

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.