2023-12-14 2:40 AM
how Mach resource required for run led display in stm32H757i evk ?
i am working on stm32H757i evk, my actual product have not external ram.
but i have run lcd display in my project.
without external ram i can run display?
my display is not more sophisticated gui, but simple data display on lcd,
please help me guide how mach ram required for my simple gui application.
Solved! Go to Solution.
2023-12-14 8:39 PM
Well that's 16 Mb (2 MB) not 8 Mb. So yes, that will get you two screen buffers, and some additional slack for icons, and resources.
2023-12-14 3:25 AM
Hello,
It depends on the size of your display and its resolution.
Please refer to the AN4861 "LCD-TFT display controller (LTDC) on STM32 MCUs"
2023-12-14 3:34 AM
i use
4” 480×800 TFT color LCD with MIPI DSI® interface and capacitive touch
panel.
so how Mach Ram need ?
2023-12-14 3:44 AM - edited 2023-12-14 3:45 AM
Again, please refer to the AN4861 "LCD-TFT display controller (LTDC) on STM32 MCUs" and section 4.2.1 Framebuffer memory size requirements and location. The details of the frame buffer size computation are there.
2023-12-14 3:49 AM
Much
At least 768KB for a frame buffer
Alternatively get a display with its own buffer.
2023-12-14 4:14 AM
i have already 8 mb extern sram are connected and i use stm32H757 microcontroller and my display is
4” 480×800 TFT color LCD with MIPI DSI® interface and capacitive touch.
and my gui is simple data display on lcd, that 8mb external ram is sufficient ?
ya need 32 mb external sdram ?
please guide me
2023-12-14 5:30 AM
8MB (64Mb) would be more than sufficient to sustain the display.
I'd probably go with 32-bit wide bus.
Cost difference for larger SDRAM might be somewhat marginal. Pick parts which ship in large volumes, and have long-term availability.
2023-12-14 8:30 PM
sorry but i have only 1M x16bit (IS61WV102416BLL-10MLI ) sram memory in my board.
that sufficient to sustain the display.?
2023-12-14 8:39 PM
Well that's 16 Mb (2 MB) not 8 Mb. So yes, that will get you two screen buffers, and some additional slack for icons, and resources.