cancel
Showing results for 
Search instead for 
Did you mean: 

Windows 10 (ed 2004) crashes (BSD) when connecting nucleo-h743zi via usb. Any suggestion? Other nucleo's are working well. (Some years ago, there was no problem with the H7).

Ggast
Associate III
 
6 REPLIES 6
Pavel A.
Evangelist III

More info, please? Does a specific Windows driver cause the crash? If yes, which one? This should be visible on the "blue screen".

-- pa

Ggast
Associate III

FAT file system.

I hesitated to provoke this again. Last time some files had been destroyed.

Ggast
Associate III

No proposal to fix the nice St-Link on the Nucleo H7 board ?

BSD: FAT file system error when plugging in

Ggast
Associate III

With Nucleo f3xx board Windows 10 starts normally. Now I additionally got a Nucleo f446 board.

With that Nucleo f446 board (got it new) and the olderH743ZI Windows crashes immediately when plugging in ( Blue Screen of Death): FAT file system error.

So I can't use those boards. (As I said, a year ago or so there was no problem, so this must have arose by some updates).

Since this is a serious issue others might experience too it would be nice if that could be fixed.

Then congratulations, you've found a exploitable Win10 2004 bug.

-- pa

Ggast
Associate III

Thank you, more details, please....