2020-09-09 05:37 AM
2020-09-09 04:33 PM
More info, please? Does a specific Windows driver cause the crash? If yes, which one? This should be visible on the "blue screen".
-- pa
2020-09-12 12:03 AM
FAT file system.
I hesitated to provoke this again. Last time some files had been destroyed.
2020-09-24 05:02 AM
No proposal to fix the nice St-Link on the Nucleo H7 board ?
BSD: FAT file system error when plugging in
2020-10-04 01:19 AM
With Nucleo f3xx board Windows 10 starts normally. Now I additionally got a Nucleo f446 board.
With that Nucleo f446 board (got it new) and the olderH743ZI Windows crashes immediately when plugging in ( Blue Screen of Death): FAT file system error.
So I can't use those boards. (As I said, a year ago or so there was no problem, so this must have arose by some updates).
Since this is a serious issue others might experience too it would be nice if that could be fixed.
2020-10-04 04:10 PM
Then congratulations, you've found a exploitable Win10 2004 bug.
-- pa
2020-10-04 11:28 PM
Thank you, more details, please....