cancel
Showing results for 
Search instead for 
Did you mean: 

Will the data of FIFO be flushed when multiple streams start simultaneously in the same DMA.

JTOM.1
Associate II

For example,One stream use FIFO and the other stream does not.

What does FIFO behave like when two streams are started at the same time?

1 REPLY 1

The streams are completely independent in this regard.

Talking about FIFO "flushing" makes sense only in P->M case. It gets "flushed" to memory either when it reaches the set threshold, or when the stream is disabled.

JW