2025-03-17 9:51 PM - edited 2025-03-17 9:58 PM
Hello,
I designed a similar board using STM32H743ZIT6 and STM32H743VIT6. (Rev. V)
The board works fine normally.
It has been in production for 3 years already.
Boards that have already been produced and shipped sometimes become unusable. (since a few months ago)
We retrieved the board and debugged it.
In the code below, it stays in Error_Handle() due to Time Out.
void SystemClock_Config(void)
{
RCC_OscInitTypeDef RCC_OscInitStruct = {0};
RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};
RCC_PeriphCLKInitTypeDef PeriphClkInitStruct = {0};
/** Supply configuration update enable
*/
HAL_PWREx_ConfigSupply(PWR_LDO_SUPPLY);
/** Configure the main internal regulator output voltage
*/
__HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE1);
while(!__HAL_PWR_GET_FLAG(PWR_FLAG_VOSRDY)) {}
/* Enable D2 domain SRAM3 Clock (0x30040000 AXI)*/
__HAL_RCC_D2SRAM3_CLK_ENABLE();
/** Macro to configure the PLL clock source
*/
HAL_PWR_EnableBkUpAccess();
__HAL_RCC_LSEDRIVE_CONFIG(RCC_LSEDRIVE_LOW);
/** Macro to configure the PLL clock source
*/
__HAL_RCC_PLL_PLLSOURCE_CONFIG(RCC_PLLSOURCE_HSE);
/** Initializes the RCC Oscillators according to the specified parameters
* in the RCC_OscInitTypeDef structure.
*/
RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI|RCC_OSCILLATORTYPE_LSI|RCC_OSCILLATORTYPE_HSE|RCC_OSCILLATORTYPE_LSE;
RCC_OscInitStruct.HSEState = RCC_HSE_ON;
RCC_OscInitStruct.LSEState = RCC_LSE_ON;
RCC_OscInitStruct.HSIState = RCC_HSI_DIV1;
RCC_OscInitStruct.HSICalibrationValue = RCC_HSICALIBRATION_DEFAULT;
RCC_OscInitStruct.LSIState = RCC_LSI_ON;
RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSE;
RCC_OscInitStruct.PLL.PLLM = 5;
RCC_OscInitStruct.PLL.PLLN = 160;
RCC_OscInitStruct.PLL.PLLP = 2;
RCC_OscInitStruct.PLL.PLLQ = 20;
RCC_OscInitStruct.PLL.PLLR = 8;
RCC_OscInitStruct.PLL.PLLRGE = RCC_PLL1VCIRANGE_2;
RCC_OscInitStruct.PLL.PLLVCOSEL = RCC_PLL1VCOWIDE;
RCC_OscInitStruct.PLL.PLLFRACN = 0;
if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
{
Error_Handler();
}
/** Initializes the CPU, AHB and APB buses clocks
*/
RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
|RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2
|RCC_CLOCKTYPE_D3PCLK1|RCC_CLOCKTYPE_D1PCLK1;
RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
RCC_ClkInitStruct.SYSCLKDivider = RCC_SYSCLK_DIV1;
RCC_ClkInitStruct.AHBCLKDivider = RCC_HCLK_DIV2;
RCC_ClkInitStruct.APB3CLKDivider = RCC_APB3_DIV2;
RCC_ClkInitStruct.APB1CLKDivider = RCC_APB1_DIV2;
RCC_ClkInitStruct.APB2CLKDivider = RCC_APB2_DIV2;
RCC_ClkInitStruct.APB4CLKDivider = RCC_APB4_DIV2;
if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_4) != HAL_OK)
{
Error_Handler();
}
PeriphClkInitStruct.PeriphClockSelection = RCC_PERIPHCLK_RTC|RCC_PERIPHCLK_USART3
|RCC_PERIPHCLK_LPUART1|RCC_PERIPHCLK_USART2
|RCC_PERIPHCLK_UART4|RCC_PERIPHCLK_UART7
|RCC_PERIPHCLK_USART6|RCC_PERIPHCLK_FDCAN
|RCC_PERIPHCLK_USART1|RCC_PERIPHCLK_UART8
|RCC_PERIPHCLK_UART5|RCC_PERIPHCLK_SDMMC
|RCC_PERIPHCLK_USB;
PeriphClkInitStruct.PLL3.PLL3M = 25;
PeriphClkInitStruct.PLL3.PLL3N = 192;
PeriphClkInitStruct.PLL3.PLL3P = 2;
PeriphClkInitStruct.PLL3.PLL3Q = 4;
PeriphClkInitStruct.PLL3.PLL3R = 2;
PeriphClkInitStruct.PLL3.PLL3RGE = RCC_PLL3VCIRANGE_0;
PeriphClkInitStruct.PLL3.PLL3VCOSEL = RCC_PLL3VCOWIDE;
PeriphClkInitStruct.PLL3.PLL3FRACN = 0;
PeriphClkInitStruct.SdmmcClockSelection = RCC_SDMMCCLKSOURCE_PLL;
PeriphClkInitStruct.FdcanClockSelection = RCC_FDCANCLKSOURCE_PLL;
PeriphClkInitStruct.Usart234578ClockSelection = RCC_USART234578CLKSOURCE_D2PCLK1;
PeriphClkInitStruct.Usart16ClockSelection = RCC_USART16CLKSOURCE_D2PCLK2;
PeriphClkInitStruct.UsbClockSelection = RCC_USBCLKSOURCE_PLL3;
PeriphClkInitStruct.RTCClockSelection = RCC_RTCCLKSOURCE_LSE;
if (HAL_RCCEx_PeriphCLKConfig(&PeriphClkInitStruct) != HAL_OK)
{
Error_Handler();
}
HAL_RCC_MCOConfig(RCC_MCO1, RCC_MCO1SOURCE_HSE, RCC_MCODIV_1);
/** Enable USB Voltage detector
*/
HAL_PWREx_EnableUSBVoltageDetector();
}
it call HAL_RCC_OscConfig() in SystemClock_Config() above.
And a timeout occurs in the part where DBP is set to 1 for LSE initialization.
__weak HAL_StatusTypeDef HAL_RCC_OscConfig(RCC_OscInitTypeDef *RCC_OscInitStruct)
{
uint32_t tickstart;
uint32_t temp1_pllckcfg, temp2_pllckcfg;
/* Check Null pointer */
if(RCC_OscInitStruct == NULL)
{
return HAL_ERROR;
}
/* Check the parameters */
assert_param(IS_RCC_OSCILLATORTYPE(RCC_OscInitStruct->OscillatorType));
/*------------------------------- HSE Configuration ------------------------*/
if(((RCC_OscInitStruct->OscillatorType) & RCC_OSCILLATORTYPE_HSE) == RCC_OSCILLATORTYPE_HSE)
{
/* Check the parameters */
assert_param(IS_RCC_HSE(RCC_OscInitStruct->HSEState));
const uint32_t temp_sysclksrc=__HAL_RCC_GET_SYSCLK_SOURCE();
const uint32_t temp_pllckselr = RCC->PLLCKSELR;
/* When the HSE is used as system clock or clock source for PLL in these cases HSE will not disabled */
if((temp_sysclksrc== RCC_CFGR_SWS_HSE) || ((temp_sysclksrc== RCC_CFGR_SWS_PLL1) && ((temp_pllckselr & RCC_PLLCKSELR_PLLSRC) == RCC_PLLCKSELR_PLLSRC_HSE)))
{
if((__HAL_RCC_GET_FLAG(RCC_FLAG_HSERDY) != 0U) && (RCC_OscInitStruct->HSEState == RCC_HSE_OFF))
{
return HAL_ERROR;
}
}
else
{
/* Set the new HSE configuration ---------------------------------------*/
__HAL_RCC_HSE_CONFIG(RCC_OscInitStruct->HSEState);
/* Check the HSE State */
if(RCC_OscInitStruct->HSEState != RCC_HSE_OFF)
{
/* Get Start Tick*/
tickstart = HAL_GetTick();
/* Wait till HSE is ready */
while(__HAL_RCC_GET_FLAG(RCC_FLAG_HSERDY) == 0U)
{
if((uint32_t) (HAL_GetTick() - tickstart ) > HSE_TIMEOUT_VALUE)
{
return HAL_TIMEOUT;
}
}
}
else
{
/* Get Start Tick*/
tickstart = HAL_GetTick();
/* Wait till HSE is disabled */
while(__HAL_RCC_GET_FLAG(RCC_FLAG_HSERDY) != 0U)
{
if((uint32_t) (HAL_GetTick() - tickstart ) > HSE_TIMEOUT_VALUE)
{
return HAL_TIMEOUT;
}
}
}
}
}
// ... //
/*------------------------------ LSE Configuration -------------------------*/
if(((RCC_OscInitStruct->OscillatorType) & RCC_OSCILLATORTYPE_LSE) == RCC_OSCILLATORTYPE_LSE)
{
/* Check the parameters */
assert_param(IS_RCC_LSE(RCC_OscInitStruct->LSEState));
/* Enable write access to Backup domain */
PWR->CR1 |= PWR_CR1_DBP;
/* Wait for Backup domain Write protection disable */
tickstart = HAL_GetTick();
while((PWR->CR1 & PWR_CR1_DBP) == 0U)
{
if((HAL_GetTick() - tickstart ) > RCC_DBP_TIMEOUT_VALUE)
{
return HAL_TIMEOUT;
}
}
/* Set the new LSE configuration -----------------------------------------*/
__HAL_RCC_LSE_CONFIG(RCC_OscInitStruct->LSEState);
/* Check the LSE State */
if((RCC_OscInitStruct->LSEState) != RCC_LSE_OFF)
{
/* Get Start Tick*/
tickstart = HAL_GetTick();
/* Wait till LSE is ready */
while(__HAL_RCC_GET_FLAG(RCC_FLAG_LSERDY) == 0U)
{
if((HAL_GetTick() - tickstart ) > RCC_LSE_TIMEOUT_VALUE)
{
return HAL_TIMEOUT;
}
}
}
else
{
/* Get Start Tick*/
tickstart = HAL_GetTick();
/* Wait till LSE is disabled */
while(__HAL_RCC_GET_FLAG(RCC_FLAG_LSERDY) != 0U)
{
if((HAL_GetTick() - tickstart ) > RCC_LSE_TIMEOUT_VALUE)
{
return HAL_TIMEOUT;
}
}
}
}
}
In other words, the timeout occurs where DBP is set to 1 in PWR_CR1 and waits.
/* Enable write access to Backup domain */
PWR->CR1 |= PWR_CR1_DBP;
/* Wait for Backup domain Write protection disable */
tickstart = HAL_GetTick();
while((PWR->CR1 & PWR_CR1_DBP) == 0U)
{
if((HAL_GetTick() - tickstart ) > RCC_DBP_TIMEOUT_VALUE)
{
return HAL_TIMEOUT;
}
}
I am curious as to why there's a timeout here, and why it waits here unlike other codes?
By any chance, does this happen when DBP is already 1 and I set it back to 1?
Finally, this symptom goes away then the battery is removed from VBAT.
Thank you for reading this article.
2025-03-17 11:47 PM
Dear @JongOk Baek ,
As the board was running for 3 Years and only recently this behavior is observed, also
the symptom goes away when the battery is removed from VBAT. it might be an issue with the power supply ( VBAT) or the state of the backup domain, it might lead to unexpected behavior. if possible, to share your schematics and also check between a working board and non-working board the status of VBAT pin / Back up domain registers and flags set/reset ?
Hope it helps you.
STOne-32.
2025-03-18 12:02 AM
Dear STOne-32,
Thanks for your reply.
First of all, there is an expression of misunderstanding.
It has been n production for 3 years, and occurs in recently produced board.
These symptoms do not appear easily.
So, I don't have the error board.
I want to comment out the waiting code.
/* Wait for Backup domain Write protection disable */
tickstart = HAL_GetTick();
while((PWR->CR1 & PWR_CR1_DBP) == 0U)
{
if((HAL_GetTick() - tickstart ) > RCC_DBP_TIMEOUT_VALUE)
{
return HAL_TIMEOUT;
}
}Without this part, it seems possible to proceed next.
Because, the other code does not wait in SystemClock_Config() function.
/** Macro to configure the PLL clock source
*/
HAL_PWR_EnableBkUpAccess();
__HAL_RCC_LSEDRIVE_CONFIG(RCC_LSEDRIVE_LOW);
It seems like it won't go into an infinite loop because of the Error_Handle().
Best regards,
JongOk, Baek