2020-05-31 09:47 AM
I have a Nucleo F103 board on which I'm playing with some code to generate a variable bit rate FSK data stream. The code seems to generate the right signal but at twice the expected frequency.
I have searched these boards and found one question for exactly the opposite, which hints that I may have misread the data sheets or not spotted some subtle detail. From what I can tell, timer 3's internal clock is the APB1 (low speed) clock. My code sets up :
I was expecting this to give me output signals with 116us or 204us cycle times - timer clocked at 1MHz - but I see half that, as if the pre-scalar is being clocked at SYSCLK instead of APB1.
What have I missed?
Solved! Go to Solution.
2020-05-31 11:17 AM
Timers' clock is 2x APB clock, if APB divider > 1, see clock diagram in RCC chapter in RM.
(self-advertisement: nr 2 at efton.sk/STM32/gotcha)
JW
2020-05-31 11:17 AM
Timers' clock is 2x APB clock, if APB divider > 1, see clock diagram in RCC chapter in RM.
(self-advertisement: nr 2 at efton.sk/STM32/gotcha)
JW
2020-05-31 12:11 PM
Ah! Yes, I can see that now. Fine documentation that it's only mentioned in a bit of small print on a busy (and thus zoomed out) diagram. Thanks.
2020-05-31 12:43 PM
It's told also in the narrative, "The timer clock frequencies..."
I admit it's easier found if you know it's there... :-D
JW