2020-04-25 05:52 AM
Hello,
i read the UM2577 pdf, the user manual for the Discovery kit with STM32G474RE MCU (B-G474E-DPOW1 board). On page 29, chapter 13.3, an audio class-D amplifier example with separate application note is mentioned. Where can i find this app note and/or the example?
Kind regards,
Greg
2020-04-27 03:15 AM
Perhaps it is also confidential, like the source code of AN5142?
https://community.st.com/s/question/0D50X0000BqAlXeSQK/an5142
Personally, it would be interesting to get further information about H-bridge PWM programming with STM32 HRTIM for Class-D amp application.
But i understand that ST also wants to sell their Class-D Amplifier IC... ;)
Are there any other app notes, manuals etc. covering PWM H-bridge (class-D) programming with MCUs, preferably from ST, anyone can recommend? Thanks in advance.
2020-05-04 04:17 AM
Hi @GregKN ,
I think that AN5142 (Class-D audio amplifier implementation on STM32 32-bit Arm® Cortex® MCUs). Right?
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.