cancel
Showing results for 
Search instead for 
Did you mean: 

Where I find examples for B-L4S5I-IOT01A Discovery kit board?

ICaci.2
Associate

Good afternoon! 

Our university bought approximatively 9 or 10 B-L4S5I-IOT01A Discovery kits for lab/projects at Embedded Systems course. I found that for this board I have no examples. I installed 30 GB of software/support package on my laptop. 

On STM32 board site is written:

Comprehensive free software libraries and examples available with the STM32Cube MCU Package

Why I cannot find examples when I create a project with STM32Cube IDE?

I want to develop some labs using FreeRTOS and wireless connection protocols without FreeRTOS , but the examples are missing.

To view the temperature from sensor mounted on the board I created an example using libraries from STM32Cube_FW_L4_V1.17.2 package

How can I add Comprehensive examples to STM32Cube IDE.?

 I am not happy with situation which create difficulties for developing labs for students. 

1 ACCEPTED SOLUTION

Accepted Solutions
Imen.D
ST Employee

Hello @Community member​ and welcome to the Community 🙂

I recommend you review the WiFi demo app showing the temperature sensor on a web page:

STM32CubeL4/Projects/B-L4S5I-IOT01A/Applications/WiFi/WiFi_HTTP_Server at master ·

You will find BSP drivers (easy-to-use) available for various sensors: STM32CubeL4/Drivers/BSP/B-L4S5I-IOT01 at master - GitHub.

You can also get inspired from available applications here: STM32CubeL4/Projects/B-L475E-IOT01A at master · GitHub

Imen

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen

View solution in original post

11 REPLIES 11
Imen.D
ST Employee

Hello @Community member​ and welcome to the Community 🙂

I recommend you review the WiFi demo app showing the temperature sensor on a web page:

STM32CubeL4/Projects/B-L4S5I-IOT01A/Applications/WiFi/WiFi_HTTP_Server at master ·

You will find BSP drivers (easy-to-use) available for various sensors: STM32CubeL4/Drivers/BSP/B-L4S5I-IOT01 at master - GitHub.

You can also get inspired from available applications here: STM32CubeL4/Projects/B-L475E-IOT01A at master · GitHub

Imen

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen
hayat
Associate III

Hi

 

If you are still looking for lab sheets on this "B-L4S5I-IOT01A Discovery kit", I can share the material.

I have developed a lab manual for an "embedded system" course using the kit in question.

The material is mainly for the educational needs of the BS level students

 

hayat
Associate III

Contents of the training manual on the "B-L4S5I-IOT01A Discovery" kit.

 

  1. Unit 01 - Introduction to C Programming 
  1. Unit 02 - Getting Started With GPIO 
  1. Unit 03 - Getting Started With EXTI 
  1. Unit 04 - Digital Interfacing (I) 
  1. Unit 04 - Digital Interfacing (II) 
  1. Unit 05 - Serial Communication (I) 
  1. Unit 05 - Serial Communication (II) 
  1. Unit 05 - Serial Communication (III) 
  1. Unit 06 - Analog Interfacing (I) 
  1. Unit 06 - Analog Interfacing (II) 
  1. Unit 07 - Counter and Timer and PWM 
  1. Unit 08 - Polling and Interrupt and DMA 
  1. Unit 09 - Getting Started With RTOS (I) 
  1. Unit 09 - Getting Started With RTOS (II) 
  1. Unit 10 - Getting Started With FSM 
  1. Unit 11 - Getting Started With Sensors (I) 
  1. Unit 11 - Getting Started With Sensors (II) 
  1. Unit 11 - Getting Started With Sensors (III) 
  1. Unit 12 - Build an IOT System (I) 
  1. Unit 12 - Build an IOT System (II) 
  1. Unit 12 - Build an IOT System (III) 
  1. Unit 13 - Cloud AWS and IOT Applications (I) 

 

  1. Appendix A - References 
  1. Appendix B - Tools Installation (STM32Cube) 
  1. Appendix C - Tools Installation (Keil-uVision) 
  1. Appendix D - Getting Started With Hardware Board 

Wow! 

I'm also trying to master the STM32 platform with the help of this particular board.

 

Where I could find these labs to try on?

I'd greatly appreciate it if you could share the lab manual for the 'B-L4S5I-IOT01A Discovery kit.' It sounds like it would be incredibly helpful. Thank you so much in advance

hayat
Associate III
 

Try the below-listed link to access the material,

 

https://drive.google.com/drive/u/2/folders/19yKII2xydTZjS4XE1g5-YpHA2sRcXnTD

 

 

Try the below listed link to access the material

 

https://drive.google.com/drive/u/2/folders/19yKII2xydTZjS4XE1g5-YpHA2sRcXnTD

 

 

Govardhini
Associate II

I can't find all the topic you have mentioned above in the provided google drive