cancel
Showing results for 
Search instead for 
Did you mean: 

when did stm start to sell H7 series MCU?

forest xu
Associate II

I have bought some H745 IC. I am sure if they are old or new

7 REPLIES 7

Take a clear, large and in-focus picture and attach.

Some of the earliest H7 perhaps 2017, the H745 2019Q1, perhaps late 2018

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
forest xu
Associate II

Hi, Tesla:

please refer to the attached photo. can you tell how many years old?

I found when heat it up. it work. when cool down, it stop work.

I am not sure if the BGA oxided

thank you

forest

That is an STM32F407IGH6 perhaps 2009 / 2019, this is not an H745

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
forest xu
Associate II

Thank you very much

:face_screaming_in_fear: :face_screaming_in_fear:

Hi,tesla:

I made mistake. please refer to the attached photo. I have the following questions.

  1. What is the version of bootloader for below st32H745 chip? and DFU version?

2. When flashing M7 large code, segment[2] fails, but when flashing M7 smaller code (not using segment[2]), it works fine.  

thank you very much.

Hi @forest xu​ ,

To identify the bootloader version, you need to refer to the section "Bootloader identification" in AN2606 STM32 microcontroller system memory boot mode.

-Amel

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Thank you !