2023-07-16 3:00 PM
Hi!
I'm using STM32F217IGT.
I want to know changing VDD anytime.
I think.
1. change firmware correction VDD(3.3V firmware or 1.8V firmware)
2. change system clock configuration void SystemClock_Config(void) in main.c
--> 7WS
Thank you!
2023-07-17 2:29 AM
If you set the system clock/waitstates for 1.8V, you can use any VDD value.
JW
2023-07-17 4:06 PM
Hi! waclawek.jan.
Thank you your answer!!
If i set 7WS, i can use any VDD value?
I added capture Table3. Number of wait sate...
It's difference Voltage range...
Thank you!
2023-07-18 7:55 AM
> If i set 7WS, i can use any VDD value?
Yes.
JW
2023-07-18 2:57 PM
Hi! waclawek.jan.
Thank you your answer!
I'll test that setting and I'll answer result.
Thank you!