Skip to main content
MNapi
Senior II
April 4, 2024
Solved

what does the status codes mean, how do you read them ?

  • April 4, 2024
  • 1 reply
  • 1294 views

here are the functions:

/**
* @brief Return the OSPI error code.
* @PAram hospi : OSPI handle
* @retval OSPI Error Code
*/
uint32_t HAL_OSPI_GetError(const OSPI_HandleTypeDef *hospi)
{
return hospi->ErrorCode;
}

/**
* @brief Return the OSPI handle state.
* @PAram hospi : OSPI handle
* @retval HAL state
*/
uint32_t HAL_OSPI_GetState(const OSPI_HandleTypeDef *hospi)
{
/* Return OSPI handle state */
return hospi->State;
}

 

I am reading

state = 2

error = 0

nowhere to find what those numbers mean.

Best answer by mƎALLEm

Hello,

Defined in stm32h7xx_hal_ospi.h header file: 

ErrorCode:

 

#define HAL_OSPI_ERROR_NONE ((uint32_t)0x00000000U) /*!< No error */
#define HAL_OSPI_ERROR_TIMEOUT ((uint32_t)0x00000001U) /*!< Timeout error */
#define HAL_OSPI_ERROR_TRANSFER ((uint32_t)0x00000002U) /*!< Transfer error */
#define HAL_OSPI_ERROR_DMA ((uint32_t)0x00000004U) /*!< DMA transfer error */
#define HAL_OSPI_ERROR_INVALID_PARAM ((uint32_t)0x00000008U) /*!< Invalid parameters error */
#define HAL_OSPI_ERROR_INVALID_SEQUENCE ((uint32_t)0x00000010U) /*!< Sequence of the state machine is incorrect */

 

State:

 

#define HAL_OSPI_STATE_RESET ((uint32_t)0x00000000U) /*!< Initial state */
#define HAL_OSPI_STATE_HYPERBUS_INIT ((uint32_t)0x00000001U) /*!< Initialization done in hyperbus mode but timing configuration not done */
#define HAL_OSPI_STATE_READY ((uint32_t)0x00000002U) /*!< Driver ready to be used */
#define HAL_OSPI_STATE_CMD_CFG ((uint32_t)0x00000004U) /*!< Command (regular or hyperbus) configured, ready for an action */
#define HAL_OSPI_STATE_READ_CMD_CFG ((uint32_t)0x00000014U) /*!< Read command configuration done, not the write command configuration */
#define HAL_OSPI_STATE_WRITE_CMD_CFG ((uint32_t)0x00000024U) /*!< Write command configuration done, not the read command configuration */
#define HAL_OSPI_STATE_BUSY_CMD ((uint32_t)0x00000008U) /*!< Command without data on-going */
#define HAL_OSPI_STATE_BUSY_TX ((uint32_t)0x00000018U) /*!< Indirect Tx on-going */
#define HAL_OSPI_STATE_BUSY_RX ((uint32_t)0x00000028U) /*!< Indirect Rx on-going */
#define HAL_OSPI_STATE_BUSY_AUTO_POLLING ((uint32_t)0x00000048U) /*!< Auto-polling on-going */
#define HAL_OSPI_STATE_BUSY_MEM_MAPPED ((uint32_t)0x00000088U) /*!< Memory-mapped on-going */
#define HAL_OSPI_STATE_ABORT ((uint32_t)0x00000100U) /*!< Abort on-going */
#define HAL_OSPI_STATE_ERROR ((uint32_t)0x00000200U) /*!< Blocking error, driver should be re-initialized */

 

 

 

1 reply

mƎALLEm
mƎALLEmBest answer
ST Technical Moderator
April 4, 2024

Hello,

Defined in stm32h7xx_hal_ospi.h header file: 

ErrorCode:

 

#define HAL_OSPI_ERROR_NONE ((uint32_t)0x00000000U) /*!< No error */
#define HAL_OSPI_ERROR_TIMEOUT ((uint32_t)0x00000001U) /*!< Timeout error */
#define HAL_OSPI_ERROR_TRANSFER ((uint32_t)0x00000002U) /*!< Transfer error */
#define HAL_OSPI_ERROR_DMA ((uint32_t)0x00000004U) /*!< DMA transfer error */
#define HAL_OSPI_ERROR_INVALID_PARAM ((uint32_t)0x00000008U) /*!< Invalid parameters error */
#define HAL_OSPI_ERROR_INVALID_SEQUENCE ((uint32_t)0x00000010U) /*!< Sequence of the state machine is incorrect */

 

State:

 

#define HAL_OSPI_STATE_RESET ((uint32_t)0x00000000U) /*!< Initial state */
#define HAL_OSPI_STATE_HYPERBUS_INIT ((uint32_t)0x00000001U) /*!< Initialization done in hyperbus mode but timing configuration not done */
#define HAL_OSPI_STATE_READY ((uint32_t)0x00000002U) /*!< Driver ready to be used */
#define HAL_OSPI_STATE_CMD_CFG ((uint32_t)0x00000004U) /*!< Command (regular or hyperbus) configured, ready for an action */
#define HAL_OSPI_STATE_READ_CMD_CFG ((uint32_t)0x00000014U) /*!< Read command configuration done, not the write command configuration */
#define HAL_OSPI_STATE_WRITE_CMD_CFG ((uint32_t)0x00000024U) /*!< Write command configuration done, not the read command configuration */
#define HAL_OSPI_STATE_BUSY_CMD ((uint32_t)0x00000008U) /*!< Command without data on-going */
#define HAL_OSPI_STATE_BUSY_TX ((uint32_t)0x00000018U) /*!< Indirect Tx on-going */
#define HAL_OSPI_STATE_BUSY_RX ((uint32_t)0x00000028U) /*!< Indirect Rx on-going */
#define HAL_OSPI_STATE_BUSY_AUTO_POLLING ((uint32_t)0x00000048U) /*!< Auto-polling on-going */
#define HAL_OSPI_STATE_BUSY_MEM_MAPPED ((uint32_t)0x00000088U) /*!< Memory-mapped on-going */
#define HAL_OSPI_STATE_ABORT ((uint32_t)0x00000100U) /*!< Abort on-going */
#define HAL_OSPI_STATE_ERROR ((uint32_t)0x00000200U) /*!< Blocking error, driver should be re-initialized */

 

 

 

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
Andrew Neil
Super User
April 4, 2024

This really ought to be stated in the function header comment; eg,

/**
* @brief Return the OSPI error code.
* @PAram hospi : OSPI handle
* @retval OSPI Error Code - one of the HAL_OSPI_ERROR_... values 
*/

 

Similarly:

/**
* @brief Return the OSPI handle state.
* @PAram hospi : OSPI handle
* @retval HAL state - one of the HAL_OSPI_STATE_... values
*/

 

Or, why not make them enums ? 

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.