2024-09-09 04:08 AM
Below is the analog waveform for the SPI clock at 12MHz. How to improve the strength of this signal and get p-p 3.3V SPI clock at 12MHz ?
"GPIO SPEED" set to the "VERY HIGH" setting. Apart from this, is there any additional settings required ?
2024-09-09 05:31 AM
GPIO speed very high is a good start.
Have you checked that you are using the correct Mode and Alternate Function for that specific SPIn peripheral?
2024-09-09 05:36 AM
Yes all that is configured correctly. Communication works fine at lower frequencies. No problems with SPI other than the strength of the clock signal at 12MHz.