2020-05-04 6:15 AM
Are you aware of ST problems with this Step 4 version.
We think, that the driver can not go to Low Level
2020-05-18 6:34 AM
Hi @SSpoh.1 ,
What do you mean by "step"? Do you mean that you are migrating from STM32F2 to STM32F4?
These are not steps, but different families of STM32 microcontroller.
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2020-05-18 6:40 AM
Stepping is the common term to describe the version/revision of silicon, and mask sets related to the IC
ie REVID within DBGMCU IDCODE
2020-05-18 6:41 AM
2020-05-18 6:45 AM
2020-05-18 9:13 AM
Need to fix the image attachment.
If the Errata attached to previous post is not sufficient you'd likely want to get with the FAE supporting your account to get some better understanding/translation of the issue.
2020-05-18 9:48 AM
Did you take an old working board with v2 chip and physically replaced for v4, and the problem appeared?
If not, why do you think you have problem with a particular version of the chip?
JW