2018-12-20 5:37 PM
Instead of using DTCMRAM or SRAM D1 domain via AXI, I set up the linker file to use D2.
In system_stm32h7xx.c I added the lines:
/* Change the switch matrix read issuing capability to 1 for the AXI D2 target (Target 2 and INI2) */
*((__IO uint32_t*)0x51003108) = 0x00000001;
*((__IO uint32_t*)0x51043108) = 0x00000001;
But executing
/* Call static constructors */
bl __libc_init_array
in startup_stm32h743xx.s a Hard Fault is thrown.
What is missing to have normal data stored in D2 domain?
Thank you for any tipps.
Solved! Go to Solution.
2018-12-20 7:19 PM
Reset_Handler:
/* Enable D2SRAM clocks in RCC_AHB2ENR */
ldr r0, =0x580244DC
ldr r1, [r0]
orr r1, #0xE0000000
str r1, [r0]
...
2018-12-20 7:13 PM
>>What is missing to have normal data stored in D2 domain? Thank you for any tips.
Enable the D2SRAM clocks? In SystemInit() prior to __libc_init_array call, or in startup.s
ie
/* Enable D2 domain SRAM3 Clock (0x30040000 AXI)*/
__HAL_RCC_D2SRAM3_CLK_ENABLE();
/* Enable SRAM1/SRAM2/SRAM3 clocks on D2 domain */
__HAL_RCC_D2SRAM1_CLK_ENABLE();
__HAL_RCC_D2SRAM2_CLK_ENABLE();
__HAL_RCC_D2SRAM3_CLK_ENABLE();
2018-12-20 7:19 PM
Reset_Handler:
/* Enable D2SRAM clocks in RCC_AHB2ENR */
ldr r0, =0x580244DC
ldr r1, [r0]
orr r1, #0xE0000000
str r1, [r0]
...
2018-12-21 6:08 AM
Great! Mastering the beast.
Any other places don't work, just in Reset_Handler only.
I spent too many hours with it, thank you.
2018-12-21 6:11 AM
If you get the Initial Stack Pointer set to unusable memory you're pretty much dead in the water. You can put a DTCMRAM address in the vector table, and subsequently load the SP with desired location/region
2018-12-21 6:17 AM
But I'm wondering about the necessity. Page 104 in RM0433 says:
Upon reset, clocks to blocks such as peripherals and some memories are disabled (except
for the SRAM, DTCM, ITCM and Flash memory).
And if I use D1 SRAM for data and work with Ethernet in D2, it works without enabling the clock for D2.
2018-12-21 7:54 AM
It is likely enabling some place else, I'd chase it down, but have more productive things to do.
2019-08-06 2:25 PM
Ibrahim Abdalkader had identified the issue here, but thread closed, so props to him. https://community.st.com/s/question/0D50X00009XkWvBSAV/stm32h7-and-heap-location
I had grepped the code base for the __HAL_RCC_D2SRAM, ST has is scattered hither-and-far, strategically it should be early, or in SystemInit() provided no dependencies on it for a stack, etc.
#ElephantInTheRoom I just remember where to look and why it is important.
2019-08-06 6:48 PM
I haven't seen this snippet of code before for the STM32H7 series part:
/* Change the switch matrix read issuing capability to 1 for the AXI D2 target (Target 2 and INI2) */
*((__IO uint32_t*)0x51003108) = 0x00000001;
*((__IO uint32_t*)0x51043108) = 0x00000001;
Can you share details around it? Is it for an errata item? Thanks.
2021-07-15 5:23 AM
In system_stm32h7xx.c, there is a coding line:
#if defined (DATA_IN_D2_SRAM)
/* in case of initialized data in D2 SRAM (AHB SRAM) , enable the D2 SRAM clock (AHB SRAM clock) */
#if defined(RCC_AHB2ENR_D2SRAM3EN)
RCC->AHB2ENR |= (RCC_AHB2ENR_D2SRAM1EN | RCC_AHB2ENR_D2SRAM2EN | RCC_AHB2ENR_D2SRAM3EN);
It would enable SRAM in D2.