2018-12-20 5:37 PM
Instead of using DTCMRAM or SRAM D1 domain via AXI, I set up the linker file to use D2.
In system_stm32h7xx.c I added the lines:
/* Change the switch matrix read issuing capability to 1 for the AXI D2 target (Target 2 and INI2) */
*((__IO uint32_t*)0x51003108) = 0x00000001;
*((__IO uint32_t*)0x51043108) = 0x00000001;But executing
/* Call static constructors */
bl __libc_init_arrayin startup_stm32h743xx.s a Hard Fault is thrown.
What is missing to have normal data stored in D2 domain?
Thank you for any tipps.
Solved! Go to Solution.
2021-07-15 5:30 AM
It is in Table "AXI interconnect register map and reset values", Reference Manual. This table shows Offset of AXI_TARG2_FN_MOD (0x3108) and AXI_INI2_FN_MOD (0x43108). Because the base address of Global Programmer View (GPV) is 0x51000000 (as Table "Register boundary addresses"), so: