cancel
Showing results for 
Search instead for 
Did you mean: 

Wait but MCU is unblocked

XooM
Associate III

I haven't been able to wait 500ms without affecting the timers for 7 days.
In this block, doesn't PB14 become "0" after 500ms?
Even if I use comment lines, it doesn't work.

Note: volatile uint32_t Counter = 0;
The "Counter" variable is incremented every 1ms with Timer16.

 

** STM32F030C6T6 I'm using.

** Own PCB board..

*** Note: Card of a working system.. There is no card design error.

 

 

if(htim->Instance==TIM16)
		{
		 Counter++;

		if(HAL_GPIO_ReadPin(GPIOC, GPIO_PIN_13)==0)
		  {
			  if(HAL_GPIO_ReadPin(GPIOA, GPIO_PIN_2)==0)
					 {
				         if(PA10_On==0)
				         {
                         HAL_GPIO_WritePin(GPIOB, GPIO_PIN_12,GPIO_PIN_RESET);
                         HAL_GPIO_WritePin(GPIOB, GPIO_PIN_14,GPIO_PIN_SET);
                         Counter=0;
                         PA10_On=1;

                         // Tick_PA10_On= HAL_GetTick();
                         // PA10_On=1;
				         }
				         else
				         {
				          if(Counter>500) // if((HAL_GetTick()-Tick_PA10_On)>=500)
							{
				        	 HAL_GPIO_WritePin(GPIOB, GPIO_PIN_14,GPIO_PIN_RESET);
				        	 Counter=501;
							}
				         }



				   	}
				else
					  {

					  	 HAL_GPIO_WritePin(GPIOB, GPIO_PIN_12,GPIO_PIN_SET);
					  }

		  }
		  else
		  {
			  HAL_GPIO_WritePin(GPIOB, GPIO_PIN_12,GPIO_PIN_RESET);

		  }
}

 

 

1 ACCEPTED SOLUTION

Accepted Solutions

@XooM wrote:

timer16 and SerialWire what do you want me to do


Ahh boy select as on my image  Chekbox on serial wire when you used debuger this is good point and select TIM16 as your application timebase , MX then for you after generate code changes delay control from systick to TIM16 and setup 1ms. No more is required. Test toggle with this

View solution in original post

60 REPLIES 60

It would rely on PC13 and PA2 being low before it gets to the timeout. And presumably you want it to turn off either way

 

Do all your INPUTs and OUTPUTs work otherwise? And it's just the sequencing logic that's broken?

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
MM..1
Chief III

Is your 

PA10_On

volatile?  When not and optimize level is more as 0 your code never will work. Optimizer remove line

PA10_On=1;

 

XooM
Associate III
PA10_On=1;

If I remove this line, PB14 will always remain in the SET position.

As long as PA2+PC13 continues to come, PB14 will be SET.

You dont ask this ? PB14 not go to 0 say is always 1.

And i recommend add volatile not remove

volatile int PA10_On = 0;

, but i mean we next 7 days try show you mistakes. Better is try help you create working code.

What you mean?

Try this code changes: in your main.c from rar

/* USER CODE BEGIN 2 */

  HAL_TIM_Base_Start_IT(&htim1);
  HAL_TIM_Base_Start_IT(&htim3);
//  HAL_TIM_Base_Start_IT(&htim14);
//  HAL_TIM_Base_Start_IT(&htim16);
//  HAL_TIM_Base_Start_IT(&htim17);
 /* Infinite loop */
  /* USER CODE BEGIN WHILE */
unint32_t out_Start[8];  //delay storage for 8 outs
  while (1)
  {
//first here from your code Q3 output handler
_Bool outx = 0;
outx = ( HAL_GPIO_ReadPin(GPIOC, GPIO_PIN_13)==0 && HAL_GPIO_ReadPin(GPIOA, GPIO_PIN_2)==0 );
outx |= (Q3_GPIO_Port->ODR&Q3_Pin)!=0 && (HAL_GetTick()-out_Start[0])<500;
if(((Q3_GPIO_Port->ODR&Q3_Pin)==0 && outx) || ((Q3_GPIO_Port->ODR&Q3_Pin)!=0 && !outx) ) {
    HAL_GPIO_WritePin(Q3_GPIO_Port, Q3_Pin, outx);
    if(outx) out_Start[0] = HAL_GetTick();
}
//next for example Q1 try you or ask
    /* USER CODE END WHILE */

    /* USER CODE BEGIN 3 */
  }
  /* USER CODE END 3 */
XooM
Associate III

I couldn't understand the code. I'm a bit of a beginner.

so I can't try it.

XooM
Associate III

 

if(htim->Instance==TIM16)
		{


		if(HAL_GPIO_ReadPin(GPIOC, GPIO_PIN_13)==0)
		  {
			  if(HAL_GPIO_ReadPin(GPIOA, GPIO_PIN_2)==0)
					 {
				         if(PA10_On==0)
				         {
                         HAL_GPIO_WritePin(GPIOB, GPIO_PIN_12,GPIO_PIN_RESET);
                         HAL_GPIO_WritePin(GPIOB, GPIO_PIN_14,GPIO_PIN_SET);

                         Tick_PA10_On = HAL_GetTick(); // Başlangıç zamanını kaydet
                         PA10_On = 1;                  // PA10 aktif duruma geçer

				         }
				         else
				         {
				        	if ((HAL_GetTick() - Tick_PA10_On) >= 500)
				        	 {
				        	  HAL_GPIO_WritePin(GPIOB, GPIO_PIN_14, GPIO_PIN_RESET);
				        	  //PA10_On = 0; // PA10 pasif duruma geçer
				        	  }

				         }

				   	}
				else
					  {

					  	 HAL_GPIO_WritePin(GPIOB, GPIO_PIN_12,GPIO_PIN_SET);
					  }

		  }
		  else
		  {
			  HAL_GPIO_WritePin(GPIOB, GPIO_PIN_12,GPIO_PIN_RESET);

		  }

where is my mistake here?
Can you fix my mistake in my code?
I want to RESET the PA10 pin after 500ms. 

Ctrl C Ctrl V and comment out timers. When it works i explain it for you.


@XooM wrote:

I couldn't understand the code. I'm a bit of a beginner.

so I can't try it.


Ctrl C Ctrl V and comment out timers. When it works i explain it for you.