2023-02-24 9:49 AM
2023-05-25 5:51 AM
Hello,
The FW solution would be enabling the interrupt of roll-over with a counter and disable the waveformoutput after reaching the value of 10 interrupts.
Otherwise, the HW solution would be: the use of single-shot mode (with PER/CMP to set/reset channel) and the Chopper to generate pulses with the number (and characteristics) you want.
Best regards.
Yassine.