cancel
Showing results for 
Search instead for 
Did you mean: 

Implementing APS12808L-3OBM HyperRam in Memory Mapped Mode on STM32H725. Does anyone have a working configuration?

MLuis.1
Associate III

I'm implementing a custom board with an APS12808L-3OBM HyperRam in Memory Mapped Mode on STM32H725, as recommended by ST to replace the S70KL1281 memory.

I'm having some problems getting the ram to respond. This is my current configuration:

static void MX_OCTOSPI2_Init(void)

{

 /* USER CODE BEGIN OCTOSPI2_Init 0 */

  BSP_OSPI_RAM_Init_t ospi_ram_init;

 /* USER CODE END OCTOSPI2_Init 0 */

 OSPIM_CfgTypeDef sOspiManagerCfg = {0};

 OSPI_HyperbusCfgTypeDef sHyperBusCfg = {0};

 /* USER CODE BEGIN OCTOSPI2_Init 1 */

  OSPI_HyperbusCmdTypeDef sCommand = { 0 };

  OSPI_MemoryMappedTypeDef sMemMappedCfg = { 0 };

 /* USER CODE END OCTOSPI2_Init 1 */

 /* OCTOSPI2 parameter configuration*/

 hospi2.Instance = OCTOSPI2;

 hospi2.Init.FifoThreshold = 4;

 hospi2.Init.DualQuad = HAL_OSPI_DUALQUAD_DISABLE;

 hospi2.Init.MemoryType = HAL_OSPI_MEMTYPE_HYPERBUS;

 hospi2.Init.DeviceSize = 24;

 hospi2.Init.ChipSelectHighTime = 4;

 hospi2.Init.FreeRunningClock = HAL_OSPI_FREERUNCLK_DISABLE;

 hospi2.Init.ClockMode = HAL_OSPI_CLOCK_MODE_0;

 hospi2.Init.WrapSize = HAL_OSPI_WRAP_NOT_SUPPORTED;

 hospi2.Init.ClockPrescaler = 2;

 hospi2.Init.SampleShifting = HAL_OSPI_SAMPLE_SHIFTING_NONE;

 hospi2.Init.DelayHoldQuarterCycle = HAL_OSPI_DHQC_ENABLE;

 hospi2.Init.ChipSelectBoundary = 23;

 hospi2.Init.DelayBlockBypass = HAL_OSPI_DELAY_BLOCK_USED;

 hospi2.Init.MaxTran = 0;

 hospi2.Init.Refresh = 400;

 if (HAL_OSPI_Init(&hospi2) != HAL_OK)

 {

  Error_Handler();

 }

 sOspiManagerCfg.ClkPort = 2;

 sOspiManagerCfg.DQSPort = 2;

 sOspiManagerCfg.NCSPort = 2;

 sOspiManagerCfg.IOLowPort = HAL_OSPIM_IOPORT_2_LOW;

 sOspiManagerCfg.IOHighPort = HAL_OSPIM_IOPORT_2_HIGH;

 if (HAL_OSPIM_Config(&hospi2, &sOspiManagerCfg, HAL_OSPI_TIMEOUT_DEFAULT_VALUE) != HAL_OK)

 {

  Error_Handler();

 }

 sHyperBusCfg.RWRecoveryTime = 4;

 sHyperBusCfg.AccessTime = 6;

 sHyperBusCfg.WriteZeroLatency = HAL_OSPI_LATENCY_ON_WRITE;

 sHyperBusCfg.LatencyMode = HAL_OSPI_FIXED_LATENCY;

 if (HAL_OSPI_HyperbusCfg(&hospi2, &sHyperBusCfg, HAL_OSPI_TIMEOUT_DEFAULT_VALUE) != HAL_OK)

 {

  Error_Handler();

 }

 /* USER CODE BEGIN OCTOSPI2_Init 2 */

  sCommand.AddressSpace = HAL_OSPI_MEMORY_ADDRESS_SPACE;

  sCommand.AddressSize = HAL_OSPI_ADDRESS_32_BITS;

  sCommand.DQSMode = HAL_OSPI_DQS_ENABLE;

  sCommand.Address = 0;

  sCommand.NbData = 1;

  if (HAL_OSPI_HyperbusCmd(&hospi2, &sCommand, HAL_OSPI_TIMEOUT_DEFAULT_VALUE) != HAL_OK)

  {

    Error_Handler();

  }

  sMemMappedCfg.TimeOutActivation = HAL_OSPI_TIMEOUT_COUNTER_DISABLE;

  if (HAL_OSPI_MemoryMapped(&hospi2, &sMemMappedCfg) != HAL_OK)

  {

    Error_Handler();

  }

 /* USER CODE END OCTOSPI2_Init 2 */

}

Does anyone have a working configuration? Any suggestions?

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
KDJEM.1
ST Employee

Hi @MLuis.1​ ,

I advise you to refer to AN5050 Getting started with Octo-SPI and Hexadeca-SPI Interface on STM32 microcontrollers application note Section 6.2 OCTOSPI configuration with STM32CubeMX and check the OCTOSPI configuration for the AP Memory.

Also, I recommend you to take a look to the Errata sheet Section 2.7 OCTOSPI and check the different case of the errata and the workaround.

I hope this help you!

Kaouthar

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

1 REPLY 1
KDJEM.1
ST Employee

Hi @MLuis.1​ ,

I advise you to refer to AN5050 Getting started with Octo-SPI and Hexadeca-SPI Interface on STM32 microcontrollers application note Section 6.2 OCTOSPI configuration with STM32CubeMX and check the OCTOSPI configuration for the AP Memory.

Also, I recommend you to take a look to the Errata sheet Section 2.7 OCTOSPI and check the different case of the errata and the workaround.

I hope this help you!

Kaouthar

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.