2022-08-05 06:26 AM
For a project, I could grab a few STM32L4R5ZI-P µC and am not sure what to connect to the 2 SMPS VDD12 pins when I do not want to provide external voltage but use the integrated LDO.
The datasheet is not quite clear on this scenario.
I have no augmented power saving needs, so the internal LDO will be fine for me.
So, can I just leave pins 70 & 142 floating, or do I have to apply some decoupling capacitors?
Cheers,
B.
Solved! Go to Solution.
2022-08-05 07:29 AM
you can leave the pins floating/unconnected
BR,
J
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2022-08-05 07:29 AM
you can leave the pins floating/unconnected
BR,
J
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2022-08-07 10:31 PM
Thank you!
2022-09-13 05:24 AM
Is that valid for SMT32L496VGY also?
When I start debugging with stm32cubeide it goes in 0x1fxxxxx and I can't continue.
2022-09-15 02:45 AM
Don't cure about it, the problem was a wrong cpu solded on the board