‎2020-11-07 08:29 AM
Hello. This is my first post here. I'm pretty unexperienced at the hardware side of MCU's and I want to debug my STM32F304P6 processor (on an unofficial board) through debugger of STM32F407VG Discovery Board. I connected SWD pins ( 2nd to CLK, 4th to DIO, GND to GND and 3v3 to 3.3V on Discovery) and unplugged CN3 headers. And I get can not find target error. Than I tried to connect 5th SWD pin with NRST on board but the result is same. I read the documentation and I don't know where am I doing wrong. Thanks
PS: I tried the same method with STM32F103 too. Result is same. Discovery board works well.
Unofficial STM32F034P6 Board:
Solved! Go to Solution.
‎2020-11-09 12:39 PM
Thanks for all the comments.
I connected BOOT0 to 3V3 STM32F03 to PC while reseting core by hand than wiped the system memory. Than took the BOOT0 to GND back and connected under system reset. Now it works well
‎2020-11-07 08:32 AM
Make sure the ST-LINK has current firmware that recognizes the F0 part, also keep the connection speed down, perhaps 1 or 2 MHz
‎2020-11-07 08:37 AM
I tried on 1.8 MHz but did not work.
‎2020-11-07 09:56 AM
> STM32f0304P6
> STM32F304P6
> STM32F034P6
Three references and three different typos.
Make sure the target board has power. The SWD connector pin 1 does not provide power.
‎2020-11-07 10:05 AM
I'm sure that board has power. I connected 3.3v via 3.3 pin of Discovery board. Not the SWD.
‎2020-11-08 12:58 AM
Would you mind giving any *precise* information? E.g. there is no 3.3V pin on the discovery board, so ...?. How did you attempt to connect (which software), what's the *precise* error message you get? "I'm sure that board has power" isn't useful at all. Whether you *think* it is powered and whether it *is* powered are two very different things. Did you verify with a voltmeter?
‎2020-11-08 02:39 AM
‎2020-11-09 05:56 AM
@Andreas Bolsch​ I did the same connections with you and tested on ST-Link Utility and STM32Cubeide by using ST Link GDB Server (sorry as I say 3.3 I mean 3 that's a terrible mistake). And having errors on both of them. I'm using latest debugger frimware on STM32 Debug+Mass Storage+VCP type. I tried on different clock speeds. Thanks for your respond
Message I get on STM32CubeIde
STMicroelectronics ST-LINK GDB server. Version 5.4.0
Copyright (c) 2019, STMicroelectronics. All rights reserved.
Starting server with the following options:
Persistent Mode : Disabled
Logging Level : 1
Listen Port Number : 61234
Status Refresh Delay : 15s
Verbose Mode : Disabled
SWD Debug : Enabled
InitWhile : Enabled
Target no device found
Error in initializing ST-LINK device.
Reason: No device found on target.
‎2020-11-09 08:48 AM
st-probe output while CN3 headers ON
Found 1 stlink programmers
serial: 303636464646333633343336344534453433303334323430
hla-serial: "\x30\x36\x36\x46\x46\x46\x33\x36\x33\x34\x33\x36\x34\x45\x34\x45\x34\x33\x30\x33\x34\x32\x34\x30"
flash: 1048576 (pagesize: 16384)
sram: 196608
chipid: 0x0413
descr: F4xx
st-probe output while STM3203 connected:
Found 1 stlink programmers
serial: 303636464646333633343336344534453433303334323430
hla-serial: "\x30\x36\x36\x46\x46\x46\x33\x36\x33\x34\x33\x36\x34\x45\x34\x45\x34\x33\x30\x33\x34\x32\x34\x30"
flash: 0 (pagesize: 0)
sram: 0
chipid: 0x074b
st-util output while STM3203 connected:
st-util
2020-11-09T19:48:22 WARN common.c: unknown chip id! 0x374b
2020-11-09T19:48:22 INFO gdb-server.c: Listening at *:4242...
‎2020-11-09 12:39 PM
Thanks for all the comments.
I connected BOOT0 to 3V3 STM32F03 to PC while reseting core by hand than wiped the system memory. Than took the BOOT0 to GND back and connected under system reset. Now it works well