cancel
Showing results for 
Search instead for 
Did you mean: 

Using STLink-V3SET in mass production

Sand_STM32_user
Associate II

We are using STM32CubeProgrammer and STLINK-V3SET to program our products on our assembly line for mass production. 

We have a couple of questions 

1) Is there a way to program using the command line or some other mechanism to keep a record of the number of devices programmed successfully or failed to program in a day?

2) Is there a mechanism using any pin on STLINK-V3SET to check that programming is successful which some other hardware can connect to keep track of flashing is successful or not 

5 REPLIES 5

Thanks. Just after posting I came across the command line option and you replied soon after. 

Is there a mechanism to monitor any hardware pin of the STLink3 to check if flashing is successful or failed ?

The usual way is to do a Verify ?

Yes the usual way is to verify which will be visible to the operator on screen. But we wanted to send flashing information to a central server which monitors every station in the assembly line 

You can do a Verify via the Command-Line