2013-08-19 3:18 AM
hello
i'm trying to make the user button working with a simple led program here is the code and please tell me what's the problem (it worked just when i keep pushing user button then make a reset): ****************** #include ''stm32f4xx.h'' #include ''stm32f4_discovery.c'' #include ''stm32f4xx_gpio.c'' #include ''stm32f4xx_rcc.c'' #include ''stm32f4xx_tim.c'' #include ''misc.c'' #include ''stm32f4xx_syscfg.c'' #include ''stm32f4xx_exti.c'' #include ''wissem.c'' int main(void) { GPIO_InitTypeDef GPIO_InitStructure; /* GPIOD Periph clock enable */ RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOD, ENABLE); /* Configure PD12, PD13, PD14 and PD15 in output pushpull mode */ GPIO_InitStructure.GPIO_Pin = GPIO_Pin_12 | GPIO_Pin_13| GPIO_Pin_14| GPIO_Pin_15; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_OUT; GPIO_InitStructure.GPIO_OType = GPIO_OType_PP; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_100MHz; GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL; GPIO_Init(GPIOD, &GPIO_InitStructure); STM_EVAL_PBInit(BUTTON_USER, BUTTON_MODE_EXTI); while(1){ if(STM_EVAL_PBGetState(BUTTON_USER) == Bit_SET ) { GPIO_WriteBit(GPIOD,GPIO_Pin_12,1); //ecrire le bit delay_ms(1000); GPIO_WriteBit(GPIOD,GPIO_Pin_12,0); //ecrire le bit delay_ms(1000); } STM_EVAL_PBGetState(BUTTON_USER); } }2013-08-19 5:10 AM
You have an EXTI interrupt handler?
If not the useSTM_EVAL_PBInit(BUTTON_USER, BUTTON_MODE_GPIO);
2013-08-20 1:56 AM
thank you it worked now u were right i miss that EXTI interrupt handler