Skip to main content
dfshea
Associate II
Mar 1, 2025 2:14 AM UTC
Question

HAL_ADC_PollForConversion gets stuck

I'm writing software that involves reading a single ADC value from my STM32H7R3V8H6, however it is getting stuck in HAL_ADC_PollForConversion(&hadc1, HAL_MAX_DELAY);.

If i switch the delay to a smaller value it runs through but it still returns a timeout.

while (1)
 {
		HAL_ADC_Start(&hadc1);
		HAL_ADC_PollForConversion(&hadc1, 100);
		adc1Data = HAL_ADC_GetValue(&hadc1);
		HAL_ADC_Stop(&hadc1);
		//readT(&engine, 0);
		//readP(&engine, 0);
 /* USER CODE END WHILE */

 /* USER CODE BEGIN 3 */
 }

static void MX_ADC1_Init(void)
{

 /* USER CODE BEGIN ADC1_Init 0 */

 /* USER CODE END ADC1_Init 0 */

 ADC_MultiModeTypeDef multimode = {0};
 ADC_ChannelConfTypeDef sConfig = {0};

 /* USER CODE BEGIN ADC1_Init 1 */

 /* USER CODE END ADC1_Init 1 */

 /** Common config
 */
 hadc1.Instance = ADC1;
 hadc1.Init.ClockPrescaler = ADC_CLOCK_ASYNC_DIV1;
 hadc1.Init.Resolution = ADC_RESOLUTION_12B;
 hadc1.Init.DataAlign = ADC_DATAALIGN_RIGHT;
 hadc1.Init.ScanConvMode = ADC_SCAN_DISABLE;
 hadc1.Init.EOCSelection = ADC_EOC_SINGLE_CONV;
 hadc1.Init.LowPowerAutoWait = DISABLE;
 hadc1.Init.ContinuousConvMode = DISABLE;
 hadc1.Init.NbrOfConversion = 1;
 hadc1.Init.DiscontinuousConvMode = DISABLE;
 hadc1.Init.ExternalTrigConv = ADC_SOFTWARE_START;
 hadc1.Init.ExternalTrigConvEdge = ADC_EXTERNALTRIGCONVEDGE_NONE;
 hadc1.Init.SamplingMode = ADC_SAMPLING_MODE_NORMAL;
 hadc1.Init.ConversionDataManagement = ADC_CONVERSIONDATA_DR;
 hadc1.Init.Overrun = ADC_OVR_DATA_PRESERVED;
 hadc1.Init.OversamplingMode = DISABLE;
 if (HAL_ADC_Init(&hadc1) != HAL_OK)
 {
 Error_Handler();
 }

 /** Configure the ADC multi-mode
 */
 multimode.Mode = ADC_MODE_INDEPENDENT;
 if (HAL_ADCEx_MultiModeConfigChannel(&hadc1, &multimode) != HAL_OK)
 {
 Error_Handler();
 }

 /** Configure Regular Channel
 */
 sConfig.Channel = ADC_CHANNEL_0;
 sConfig.Rank = ADC_REGULAR_RANK_1;
 sConfig.SamplingTime = ADC_SAMPLETIME_2CYCLES_5;
 sConfig.SingleDiff = ADC_SINGLE_ENDED;
 sConfig.OffsetNumber = ADC_OFFSET_NONE;
 sConfig.Offset = 0;
 sConfig.OffsetSign = ADC_OFFSET_SIGN_NEGATIVE;
 if (HAL_ADC_ConfigChannel(&hadc1, &sConfig) != HAL_OK)
 {
 Error_Handler();
 }
 /* USER CODE BEGIN ADC1_Init 2 */

 /* USER CODE END ADC1_Init 2 */

}
This topic has been closed for replies.

17 replies

Karl Yamashita
Principal
Mar 1, 2025 3:13 AM UTC

HAL_MAX_DELAY = 49.7 Days! 

So if you wait for almost 50 days, the function will eventually return.

Typically 100ms is more than enough for a timeout.

 

How do you know if it return a timeout? You're not checking the return value.

HAL_StatusTypeDef hal_status = HAL_ADC_PollForConversion(&hadc1, 100);
	if(hal_status == HAL_ERROR)
	{
		// error handler
	}
	else if(hal_status == HAL_TIMEOUT)
	{
		// timeout handler
	}
	// get adc value

 

If a reply has proven helpful, click on Accept as Solution so that it'll show at top of the post.CAN Jammer an open source CAN bus hacking toolCANableV3 Open Source
dfshea
dfsheaAuthor
Associate II
Mar 1, 2025 3:38 AM UTC

Hm, 50 days is a bit much to see if it times out, so I reduced the delay to 100ms and added a return variable and confirmed that it is indeed returning HAL_TIMEOUT. 

 

I also did some digging and found where in the function it's getting stuck:

 tickstart = HAL_GetTick();

 /* Wait until End of unitary conversion or sequence conversions flag is raised */
 while ((hadc->Instance->ISR & tmp_Flag_End) == 0UL)
 {
 /* Check if timeout is disabled (set to infinite wait) */
 if (Timeout != HAL_MAX_DELAY)
 {
 if (((HAL_GetTick() - tickstart) > Timeout) || (Timeout == 0UL))
 {
 /* New check to avoid false timeout detection in case of preemption */
 if ((hadc->Instance->ISR & tmp_Flag_End) == 0UL)
 {
 /* Update ADC state machine to timeout */
 SET_BIT(hadc->State, HAL_ADC_STATE_TIMEOUT);

 /* Process unlocked */
 __HAL_UNLOCK(hadc);

 return HAL_TIMEOUT;
 }
 }
 }
 }

dfshea_0-1740800326794.png

 

Karl Yamashita
Principal
Mar 4, 2025 10:12 PM UTC

What's your definition of stuck? Because if you return a timeout, then how can it be stuck?

If a reply has proven helpful, click on Accept as Solution so that it'll show at top of the post.CAN Jammer an open source CAN bus hacking toolCANableV3 Open Source
ST Technical Moderator
Mar 4, 2025 9:50 AM UTC

Hello @dfshea 

Did you confirm an ADC calibration before starting the conversion please? 

Did you check to compare your implementation with the example below?

 Projects/NUCLEO-H7S3L8/Examples/ADC/ADC_SingleConversion_TriggerSW

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Saket_Om
dfshea
dfsheaAuthor
Associate II
Mar 4, 2025 9:31 PM UTC

@Saket_Om, I forgot to do the calibration, I wasn't sure if it was necessary or not. However I just tried doing the calibration and it gets stuck there as well. It gets stuck in this loop:

while (LL_ADC_IsCalibrationOnGoing(hadc->Instance) != 0UL)
 {
 wait_loop_index++;
 if (wait_loop_index >= ADC_CALIBRATION_TIMEOUT)
 {
 /* Update ADC state machine to error */
 ADC_STATE_CLR_SET(hadc->State,
 HAL_ADC_STATE_BUSY_INTERNAL,
 HAL_ADC_STATE_ERROR_INTERNAL);

 /* Process unlocked */
 __HAL_UNLOCK(hadc);

 return HAL_ERROR;
 }
 }
Chris21
Associate II
Mar 4, 2025 9:57 PM UTC

Where is the code that enables the ADC peripheral clock?

Are your ADC configuration registers all zeroes? 

.
dfshea
dfsheaAuthor
Associate II
Mar 4, 2025 9:59 PM UTC

@Chris21 It's this code here right? (I could be wrong, this was autogenerated)

static void MX_ADC1_Init(void)
{

 /* USER CODE BEGIN ADC1_Init 0 */

 /* USER CODE END ADC1_Init 0 */

 ADC_MultiModeTypeDef multimode = {0};
 ADC_ChannelConfTypeDef sConfig = {0};

 /* USER CODE BEGIN ADC1_Init 1 */

 /* USER CODE END ADC1_Init 1 */

 /** Common config
 */
 hadc1.Instance = ADC1;
 hadc1.Init.ClockPrescaler = ADC_CLOCK_ASYNC_DIV1;
 hadc1.Init.Resolution = ADC_RESOLUTION_12B;
 hadc1.Init.DataAlign = ADC_DATAALIGN_RIGHT;
 hadc1.Init.ScanConvMode = ADC_SCAN_DISABLE;
 hadc1.Init.EOCSelection = ADC_EOC_SINGLE_CONV;
 hadc1.Init.LowPowerAutoWait = DISABLE;
 hadc1.Init.ContinuousConvMode = DISABLE;
 hadc1.Init.NbrOfConversion = 1;
 hadc1.Init.DiscontinuousConvMode = DISABLE;
 hadc1.Init.ExternalTrigConv = ADC_SOFTWARE_START;
 hadc1.Init.ExternalTrigConvEdge = ADC_EXTERNALTRIGCONVEDGE_NONE;
 hadc1.Init.SamplingMode = ADC_SAMPLING_MODE_NORMAL;
 hadc1.Init.ConversionDataManagement = ADC_CONVERSIONDATA_DR;
 hadc1.Init.Overrun = ADC_OVR_DATA_PRESERVED;
 hadc1.Init.OversamplingMode = DISABLE;
 if (HAL_ADC_Init(&hadc1) != HAL_OK)
 {
 Error_Handler();
 }

 /** Configure the ADC multi-mode
 */
 multimode.Mode = ADC_MODE_INDEPENDENT;
 if (HAL_ADCEx_MultiModeConfigChannel(&hadc1, &multimode) != HAL_OK)
 {
 Error_Handler();
 }

 /** Configure Regular Channel
 */
 sConfig.Channel = ADC_CHANNEL_0;
 sConfig.Rank = ADC_REGULAR_RANK_1;
 sConfig.SamplingTime = ADC_SAMPLETIME_640CYCLES_5;
 sConfig.SingleDiff = ADC_SINGLE_ENDED;
 sConfig.OffsetNumber = ADC_OFFSET_NONE;
 sConfig.Offset = 0;
 sConfig.OffsetSign = ADC_OFFSET_SIGN_NEGATIVE;
 if (HAL_ADC_ConfigChannel(&hadc1, &sConfig) != HAL_OK)
 {
 Error_Handler();
 }
 /* USER CODE BEGIN ADC1_Init 2 */

 /* USER CODE END ADC1_Init 2 */

}
Karl Yamashita
Principal
Mar 4, 2025 10:18 PM UTC

The ADC clock is enable from calling  MX_ADC1_Init>HAL_ADC_Init>HAL_ADC_MspInit

If a reply has proven helpful, click on Accept as Solution so that it'll show at top of the post.CAN Jammer an open source CAN bus hacking toolCANableV3 Open Source
Chris21
Associate II
Mar 4, 2025 10:04 PM UTC

Somewhere you need something like:

 


/* Peripheral clock enable */
__HAL_RCC_ADC_CLK_ENABLE();

 

Also GPIO pins configured for analog mode.

.
dfshea
dfsheaAuthor
Associate II
Mar 4, 2025 10:10 PM UTC

I confirmed the pins are in analog mode. And this may be a foolish question but when I try to call __HAL_RCC_ADC_CLK_ENABLE() it says there is an undefined reference to it. Is there another HAL library I need to include in the main.c file? Thank you again for your help!

Chris21
Associate II
Mar 4, 2025 10:26 PM UTC

Looks like the H7 is a bit different as far as the ADC Clock, it's set in RCC domain 3 kernel clock configuration register (RCC_D3CCIPR):

Chris21_0-1741127127185.png

 

Chris21_1-1741127166620.png

 

.