2020-08-13 5:12 AM
Hello,
Is it possible to use the LSE clock 32.768 KHz as external clock source for TIMxx on the STM32L4 series ?
I have an application running on STM32L1 and using external ****-source mode 2 for TIM10 as described in Figure 131 of the Reference Manual RM0038. I would like to port this application to the STM32L4 but I'm not sure it's possible, I can't find the equivalent diagram in the reference manual RM0351.
Regards,
Zafi
2020-08-13 5:39 AM
Read then TIM2_OR1/TIM15_OR1/TIM16_OR1 registers description.
JW
2020-08-13 6:50 AM
Thanks for the answer.
I'm going to follow this path.
Regards,
Zafi.
2020-08-20 3:20 AM
LSE can be used as clock source:
TIM15->OR1 |= TIM15_OR1_TI1_RMP;
Thanks for the advice.