2017-08-08 5:36 AM
Hi,
The problem is when using USB VCP under Windows 10 on the Nucleo f746 board. The COM port is not open. When connecting to Windows 7 COM port opens.I tried to board Nucleo l432. Works under Windows 7 and Windows 10.
2019-04-11 1:45 AM
Hello CanhNguyen,
Same situation here, but I found another source of variability.
The VCP only works if I use the Windows API directly (C++ program)
So the Teraterm terminal works, but the dotnet based YAT terminal dont.
I hope this can help ST engineers to fix it.
2019-04-27 12:26 PM
Hi,
I also encountered this problem today - couldn't open the port in putty, got the "unable to configure the port" error too.
In my case, I had to uninstall the device driver (in device manager, uninstall device & remove installed driver).
Unplugged and plugged again and it installed some generic driver and it works - it had stm32 driver before.
2019-05-29 12:41 AM
have same problem
2019-09-15 3:01 PM
I had the same problem with my custom board with f405 MCU. The VCP was detected by win10, and drivers was ok.
More than that, i was able to open COM port with Termite terminal. But my host app (based on .net) could`t open it.
Same thing was with Qt based host app (unsupported operation error was appeared).
Fix with GET and SET line coding from Ant M helped.
Thanks!
2021-02-01 11:51 PM
I got the same kind of problem when migrating from Workbench to CubeIDE:
I already had memcpy(&dwDTERate,&pbuf[0],4); in CDC_SET_LINE_CODING case, which was enough under workbench.
In order to get the same project working on CubeIDE, it has been necessary to change the definition of dwDTERate from uint32_t to uint_64t, changed the size of the memcpy from 4 to 7, and added memcpy(&pbuf[0],&dwDTERate,7); back in CDC_GET_LINE_CODING case
Thanks for the discussion who helped me focus on where the problem was...
JYL