USART running 7N1.
My STM32F429 must interface an old modbus system running 7N1 on a RS422 bus, as slave. However, I can't see how to setup the STM32 as 7bit, NONE, 1 stopbit - not in Qube, not be registeres direct. Is this true ?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2021-12-13 2:09 AM
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2021-12-13 2:32 AM
"7N1" usually means 1 start bit, and I haven't seen any UART / RS232 like interface without a start bit in the last 20 years - but I haven't seen all! ;)
Anyway, I can't check the F429, but I just see that only the newer STMs have the 7N1 options (checked: STM32G4, STM32F7 ref manuals).
So that might get tricky, if you cannot switch the STM, on the other hand surely possible, as Modbus is rather slow (9k6?).
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2021-12-13 2:46 AM
"7N1" means: 7 data, no parity and 1 stop bit. All uart communication uses 1 start bit - this has allways been so. But that is not the question.
How do I setup the STM32F429 to read the incomming modus with the framing 7N1, without getting framing errors, etc.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2021-12-13 3:58 AM
bit 7 will act as your stop bit when sending and receiving single bytes. When sending and receiving multi-bytes, you will need to think of all the data as one big bit string and use it in 7-bit chunks. the extra stop bits shouldn't be a big problem.
You can also switch to one of the STM32's MCUs that support 7-bit UART (eg STM32F7,H7,L4)
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2021-12-13 5:42 AM
Ok, thanks for the reply. But.... the incomming data stream is 7N1 - which means (if the STM is programmed to 8 data, No parity) the incomming stop bit databit will be treated as the 8th - and the STM uart will be missing a stopbit - which will be a framing error doc according to Reference manual RM0090, page 977: "The stop bit is not recognized on reception at the expected time". A quick test gives USART_SR_FE - framing errors.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2021-12-13 6:09 AM
The UART in the STM32F4 can have either 8 or 9 data bits (including parity). 7-N-1 is not a supported configuration.
See the USART_CR1 register for details.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2021-12-13 6:31 AM
This should work if you set up the STM's UART without a stop bit, as @Muhammed G�ler​ proposed.
Just mask the last bit (MSB) of each received byte.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2021-12-13 6:37 AM
It is not possible to set up a UART on the STM32F4 without a stop bit.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2021-12-13 6:37 AM
Usart can't be setup without stopbits. I was looking for confirmation of my setup and the errors I see, so thanks to TDK for Your answer.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2021-12-13 6:51 AM
Oops, my bad. I'd better shut up about controllers I don't know...