cancel
Showing results for 
Search instead for 
Did you mean: 

Stm32f429 disco integration with finger print sensor using spi

Abhishek_nr
Associate II

Hello..

I am using STM32F429 Disco Board in which I am trying to interface finger print sensor NB65210 of next biometric using spi and I need to read the finger print data I have a example code in which it is reading properly but it is not reading when I configured for myself l, I have selected proper clock, spi pins, Chip select nreset, nawake, the library which ever they have given I have not modified NBdeviceInitializationA  it is getting nbok but after that stocking and giving error code for all library function what will the issue can anyone suggest the solution...

1 REPLY 1
Andrew Neil
Super User

@Abhishek_nr wrote:

I have a example code in which it is reading properly but it is not reading when I configured for myself l


So carefully compare & contrast your implementation against the working one.

Have you checked the interface lines with an oscilloscope and/or logic analyser to see what's actually happening on the wires?

 


@Abhishek_nr wrote:

finger print sensor NB65210 


Please post a link to its documentation.

Please post your schematic.

See: How to write your question to maximize your chances to find a solution

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.