cancel
Showing results for 
Search instead for 
Did you mean: 

USART-5 on STM32 LoRa

sgabran
Associate III

Hi

We are using the DISCO-L072CZ-LRWAN1.

USART-5 uses pin PB3 for Tx, is this pin not available on the LoRa development kit ?

Is there a way to re-route the USART-5 Tx pin or access it ?

thanks

1 ACCEPTED SOLUTION

Accepted Solutions
RhSilicon
Lead

UM2115:

The B-L072Z-LRWAN1 Discovery kit embeds the CMWX1ZZABZ-091 LoRa®/Sigfox™
module (Murata)
 
Apparently this pin (PB3) is not available:
 

View solution in original post

2 REPLIES 2
RhSilicon
Lead

UM2115:

The B-L072Z-LRWAN1 Discovery kit embeds the CMWX1ZZABZ-091 LoRa®/Sigfox™
module (Murata)
 
Apparently this pin (PB3) is not available:
 

Once upon a time I made a post highlighting all the pins, but the forum transition seems to have destroyed that. There are about 3 escapable UART as I recall. You might have to split a UART to get both TX and RX from different ones.

There's a finite number of pins on the WLCSP and escaping from the Murata module.

PB3 is used internally for the Radio's SPI connection

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..