2024-09-11 10:24 AM - last edited on 2024-09-16 8:09 AM by mƎALLEm
Hello, so I am completely new to working with STM boards in general.
I just got a brand new stm32f446re board, and I tried to upload some code to it through Linux. And I do mean brand new, I haven't uploaded or downloaded any code to it before this attempt. However, when I attempted to do so, I got an error message:
"WARN common.c: unknown chip id! 0x421"
So, I looked around for a bit and tried a simple command: st-info --probe to see some internal stuff on it. But I was told this:
"No such file or directory
version:V2J33S25
serial: 066DFF534871754867255336
flash: 0 (pagesize: 0)
sram: 0
chipid: 0x421"
After spending roughly about two weeks trying to find stuff online, I couldn't figure out anything on what to do. So, I am very much open to suggestions if anybody knows anything about this error.
Thank you very much in advance for any help.
Solved! Go to Solution.
2024-09-16 8:59 AM
@waclawek.jan wrote:I don't think the error messages we've seen from the st-link-project's utilities are related to the mbed tools used to compile/generate .bin.
Indeed.
It looks like the st-link-project's utilities are communicating successfully with the ST-Link, but the ST-Link is not communicating with the Target MCU.
@waclawek.jan wrote:I maintain that those utilities are of an obsolete version and/or incorrectly installed.
Plausible - and that was also @Tesla DeLorean's feeling, I think.
@Odega Where did the "WARN common.c: unknown chip id! 0x421" message (mentioned in the OP) come from?
2024-09-16 9:05 AM
That has disappeared on its own. A professor I talked to tried to use St-link GUI to get around the chip ID unknown problem. So perhaps that got rid of that particular issue. But now we have this one.
Side note, I didn't know that the unknown chip id error stopped showing up until you mentioned it XD.
2024-09-16 9:06 AM
@Odega wrote:The rover-stm project is a file within directories.
In Linux, everything is a file - so that really tells us nothing!
@Odega wrote:Right now, the project is to just drive a rover.
But where did you obtain it? Is it a known-good project for the Nucleo board you have?
@Odega wrote:Since we haven't fully implemented the GPS into it yet, we are just using hardware tools to drive the device.
Who is "we" ?
If there is a team on this, then surely someone must have a working setup with all the tools necessary to build and download code? Surely, they can help you?
@Odega wrote:For reference, I have pulled the microprocessor off of the project and disconnected it from everything and still get the issue.
So the Nucleo board isn't actually "brand new" - it could be damaged.
2024-09-16 9:17 AM
@Odega wrote:I didn't know that the unknown chip id error stopped showing up until you mentioned it XD.
Looks like it comes from those st-link utilities:
As noted in that thread, they are 3rd-party utilities - nothing to do with ST.
It looks like that ID comes from the Target chip, so reading it requires a working SWD link.
As you now don't have a working SWD link, that would explain why you no longer get that message.
This suggests that something has been reconfigured and/or broken on your Nucleo board.
2024-09-16 9:17 AM
I don't know if the project is good for the Nucleo board. It's what has been used for at least four years now.
By "we" I mostly meant the people who worked on this project in the past. As much as I wish I had team members to help me, I am all alone on this project. The only other person helping is my professor whose name is on this research project.
The board is brand new. For curiosity's sake, I did try to plug the board into all the other circuitry after my professor showed me the GUI trick. However, it still didn't work. So I don't think that is the issue.
2024-09-16 9:21 AM
@Andrew Neil wrote:
@waclawek.jan wrote:I maintain that those utilities are of an obsolete version and/or incorrectly installed.
Plausible - and that was also @Tesla DeLorean's feeling, I think.
https://github.com/stlink-org/stlink/issues/1241#issuecomment-1366964332
As already noted, it's a 3rd-party project - so you need to take issues up with them.